This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3354: LCD SGX issue

Part Number: AM3354

Tool/software: Linux

I am working on a board which uses an AM3354.
There is a LCD display which is used with a QT app.
I am seeing a behavior where apparently randomly, the LCD screen goes to garbled.

Whenever this problem happens, there is a lot of SGX messages being dumped to the kernel log as following.

[ 26.305950] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[ 26.305978] PVR_K: SGX debug (SGX_DDK_Linux_CustomerTI sgxddk 19 1.9@2188537)
[ 26.305997] PVR_K: (P0) EUR_CR_CORE_ID: 01120000
[ 26.306013] PVR_K: (P0) EUR_CR_CORE_REVISION: 00010205
[ 26.306028] PVR_K: (P0) EUR_CR_EVENT_STATUS: 00000000
[ 26.306044] PVR_K: (P0) EUR_CR_EVENT_STATUS2: 00000010
[ 26.306059] PVR_K: (P0) EUR_CR_BIF_CTRL: 00000000
[ 26.306073] PVR_K: (P0) EUR_CR_BIF_INT_STAT: 00000000
[ 26.306088] PVR_K: (P0) EUR_CR_BIF_FAULT: 00000000
[ 26.306103] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[ 26.306119] PVR_K: (P0) EUR_CR_CLKGATECTL: 00222220
[ 26.306143] PVR_K: (P0) EUR_CR_PDS_PC_BASE: 003000EC
[ 26.306165] PVR_K: Flip Command Complete Data 0 for display device 1:
[ 26.306180] PVR_K: SGX Host control:
[ 26.306196] PVR_K: (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[ 26.306214] PVR_K: (HC-10) 0x00000001 0x00000000 0x0000000A 0x00030D40
[ 26.306233] PVR_K: (HC-20) 0x00000000 0x00000001 0x00000001 0x00000000
[ 26.306251] PVR_K: (HC-30) 0x00000000 0x00001ED8 0x5828EDB0 0x00000000
[ 26.306269] PVR_K: (HC-40) 0x00000000 0x00000000 0x27110194 0x0F0000E6
[ 26.306284] PVR_K: SGX TA/3D control:
[ 26.306300] PVR_K: (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[ 26.306318] PVR_K: (T3C-10) 0x00000000 0x00000000 0x00000002 0x00000000
[ 26.306336] PVR_K: (T3C-20) 0x00000000 0x00000000 0x00000000 0x00000000
[ 26.306354] PVR_K: (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[ 26.306372] PVR_K: (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[ 26.306390] PVR_K: (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[ 26.306408] PVR_K: (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[ 26.306425] PVR_K: (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[ 26.306444] PVR_K: (T3C-80) 0x00000000 0x00000000 0x0F0AD55C 0x0F000000
[ 26.306462] PVR_K: (T3C-90) 0x8E05C000 0x0F08C000 0x0F0AD55C 0x0F08B920
[ 26.306480] PVR_K: (T3C-A0) 0x0F00AEA0 0x00000000 0x00000000 0x00000000
[ 26.306510] PVR_K: (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[ 26.306528] PVR_K: (T3C-C0) 0x00000000 0x00000000 0x00000000 0x00000000
[ 26.306547] PVR_K: (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000
[ 26.306566] PVR_K: (T3C-E0) 0x0F00A420 0x0F00A740 0x0F08B000 0x0F08B000
[ 26.306584] PVR_K: (T3C-F0) 0x00000000 0x000006B1 0x000006B1 0x00000000
[ 26.306604] PVR_K: (T3C-100) 0x00000002 0x00000000 0xDCC34420 0x00000000
[ 26.306622] PVR_K: (T3C-110) 0x00000000 0x23030000 0x33110180 0x0F0000CD
[ 26.306639] PVR_K: SGX Kernel CCB WO:0x28 RO:0x28
[ 26.341782] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[ 26.341812] PVR_K: SGX debug (SGX_DDK_Linux_CustomerTI sgxddk 19 1.9@2188537)
[ 26.341841] PVR_K: (P0) EUR_CR_CORE_ID: 01120000
[ 26.341857] PVR_K: (P0) EUR_CR_CORE_REVISION: 00010205
[ 26.341872] PVR_K: (P0) EUR_CR_EVENT_STATUS: 20000000
[ 26.341887] PVR_K: (P0) EUR_CR_EVENT_STATUS2: 00000010
[ 26.341902] PVR_K: (P0) EUR_CR_BIF_CTRL: 00000000
[ 26.341917] PVR_K: (P0) EUR_CR_BIF_INT_STAT: 00000000
[ 26.341932] PVR_K: (P0) EUR_CR_BIF_FAULT: 00000000
[ 26.341947] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[ 26.341963] PVR_K: (P0) EUR_CR_CLKGATECTL: 00222220
[ 26.341977] PVR_K: (P0) EUR_CR_PDS_PC_BASE: 00000000
[ 26.342001] PVR_K: Flip Command Complete Data 0 for display device 1:
[ 26.342017] PVR_K: SGX Host control:
[ 26.342033] PVR_K: (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[ 26.342051] PVR_K: (HC-10) 0x00000001 0x00000001 0x0000000A 0x00030D40
[ 26.342069] PVR_K: (HC-20) 0x00000000 0x00000000 0x00000003 0x00000000
[ 26.342096] PVR_K: (HC-30) 0x00000000 0x00001EEB 0x5CDDC330 0x00000000
[ 26.342115] PVR_K: (HC-40) 0x00000000 0x00000000 0x27110194 0x0F0000E6
[ 26.342129] PVR_K: SGX TA/3D control:
[ 26.342146] PVR_K: (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[ 26.342164] PVR_K: (T3C-10) 0x00000000 0x00000000 0x00000002 0x00000000
[ 26.342182] PVR_K: (T3C-20) 0x00000000 0x00000000 0x00000000 0x00000000
[ 26.342199] PVR_K: (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[ 26.342218] PVR_K: (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[ 26.342236] PVR_K: (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[ 26.342253] PVR_K: (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[ 26.342271] PVR_K: (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[ 26.342290] PVR_K: (T3C-80) 0x00000000 0x00000000 0x0F0AD518 0x0F000000
[ 26.342308] PVR_K: (T3C-90) 0x8E05C000 0x0F08C540 0x0F0AD518 0x0F08B920
[ 26.342326] PVR_K: (T3C-A0) 0x0F00AEA0 0x00000000 0x00000000 0x00020000
[ 26.342344] PVR_K: (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[ 26.342363] PVR_K: (T3C-C0) 0x00000000 0x00000000 0x00000001 0x00000000
[ 26.342381] PVR_K: (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000
[ 26.342400] PVR_K: (T3C-E0) 0x0F00A420 0x0F00A740 0x0F08B000 0x0F08B000
[ 26.342418] PVR_K: (T3C-F0) 0x00000000 0x000006B1 0x000006B1 0x00000001
[ 26.342437] PVR_K: (T3C-100) 0x00000003 0x00000003 0xDCC34420 0x00000001
[ 26.342456] PVR_K: (T3C-110) 0x00000000 0x23030000 0x33110180 0x0F0000CD
[ 26.342472] PVR_K: SGX Kernel CCB WO:0x2D RO:0x2C
[ 60.654785] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[ 60.654813] PVR_K: SGX debug (SGX_DDK_Linux_CustomerTI sgxddk 19 1.9@2188537)
[ 60.654833] PVR_K: (P0) EUR_CR_CORE_ID: 01120000
[ 60.654848] PVR_K: (P0) EUR_CR_CORE_REVISION: 00010205
[ 60.654874] PVR_K: (P0) EUR_CR_EVENT_STATUS: 00000000
[ 60.654890] PVR_K: (P0) EUR_CR_EVENT_STATUS2: 00000010
[ 60.654905] PVR_K: (P0) EUR_CR_BIF_CTRL: 00000000
[ 60.654919] PVR_K: (P0) EUR_CR_BIF_INT_STAT: 00000000
[ 60.654934] PVR_K: (P0) EUR_CR_BIF_FAULT: 00000000
[ 60.654950] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[ 60.654965] PVR_K: (P0) EUR_CR_CLKGATECTL: 00222220
[ 60.654980] PVR_K: (P0) EUR_CR_PDS_PC_BASE: 00300D2C
[ 60.655000] PVR_K: Flip Command Complete Data 0 for display device 1:
[ 60.655016] PVR_K: SGX Host control:
[ 60.655032] PVR_K: (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[ 60.655050] PVR_K: (HC-10) 0x00000002 0x00000001 0x0000000A 0x00030D40
[ 60.655068] PVR_K: (HC-20) 0x00000000 0x00000001 0x00000001 0x00000000
[ 60.655087] PVR_K: (HC-30) 0x00000000 0x0000A4F3 0x5CE34170 0x00000000
[ 60.655105] PVR_K: (HC-40) 0x00000000 0x00000000 0x27110194 0x0F0000E6
[ 60.655120] PVR_K: SGX TA/3D control:
[ 60.655136] PVR_K: (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[ 60.655154] PVR_K: (T3C-10) 0x00000000 0x00000000 0x00000002 0x00000000
[ 60.655172] PVR_K: (T3C-20) 0x00000000 0x00000000 0x00000000 0x00000000
[ 60.655190] PVR_K: (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[ 60.655208] PVR_K: (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[ 60.655226] PVR_K: (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[ 60.655244] PVR_K: (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[ 60.655261] PVR_K: (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[ 60.655280] PVR_K: (T3C-80) 0x00000000 0x00000000 0x0F0AD55C 0x0F000000
[ 60.655299] PVR_K: (T3C-90) 0x8E05C000 0x0F08D500 0x0F0AD55C 0x0F08B920
[ 60.655317] PVR_K: (T3C-A0) 0x0F00AEA0 0x00000000 0x00000000 0x00000000
[ 60.655334] PVR_K: (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[ 60.655353] PVR_K: (T3C-C0) 0x00000000 0x00000000 0x00000002 0x00000000
[ 60.655372] PVR_K: (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000
[ 60.655390] PVR_K: (T3C-E0) 0x0F00A420 0x0F00A740 0x0F08B000 0x0F08B000
[ 60.655408] PVR_K: (T3C-F0) 0x00000000 0x000006B1 0x000006B1 0x00000000
[ 60.655428] PVR_K: (T3C-100) 0x00000002 0x00000000 0xDCDCE420 0x00000002
[ 60.655446] PVR_K: (T3C-110) 0x00000000 0x23030000 0x33110180 0x0F0000CD
[ 60.655463] PVR_K: SGX Kernel CCB WO:0x35 RO:0x35
[ 120.653917] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[ 120.653943] PVR_K: SGX debug (SGX_DDK_Linux_CustomerTI sgxddk 19 1.9@2188537)
[ 120.653962] PVR_K: (P0) EUR_CR_CORE_ID: 01120000
[ 120.653978] PVR_K: (P0) EUR_CR_CORE_REVISION: 00010205
[ 120.654003] PVR_K: (P0) EUR_CR_EVENT_STATUS: 00000000
[ 120.654018] PVR_K: (P0) EUR_CR_EVENT_STATUS2: 00000010
[ 120.654033] PVR_K: (P0) EUR_CR_BIF_CTRL: 00000000
[ 120.654048] PVR_K: (P0) EUR_CR_BIF_INT_STAT: 00000000
[ 120.654063] PVR_K: (P0) EUR_CR_BIF_FAULT: 00000000
[ 120.654078] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[ 120.654093] PVR_K: (P0) EUR_CR_CLKGATECTL: 00222220
[ 120.654109] PVR_K: (P0) EUR_CR_PDS_PC_BASE: 00301384
[ 120.654130] PVR_K: Flip Command Complete Data 0 for display device 1:
[ 120.654145] PVR_K: SGX Host control:
[ 120.654161] PVR_K: (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[ 120.654180] PVR_K: (HC-10) 0x00000003 0x00000001 0x0000000A 0x00030D40
[ 120.654198] PVR_K: (HC-20) 0x00000000 0x00000001 0x00000001 0x00000000
[ 120.654217] PVR_K: (HC-30) 0x00000000 0x00018F51 0x71570100 0x00000000
[ 120.654235] PVR_K: (HC-40) 0x00000000 0x00000000 0x27110194 0x0F0000E6
[ 120.654250] PVR_K: SGX TA/3D control:
[ 120.654266] PVR_K: (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[ 120.654284] PVR_K: (T3C-10) 0x00000000 0x00000000 0x00000002 0x00000000
[ 120.654302] PVR_K: (T3C-20) 0x00000000 0x00000000 0x00000000 0x00000000
[ 120.654320] PVR_K: (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[ 120.654338] PVR_K: (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[ 120.654356] PVR_K: (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[ 120.654374] PVR_K: (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[ 120.654392] PVR_K: (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[ 120.654411] PVR_K: (T3C-80) 0x00000000 0x00000000 0x0F0AD518 0x0F000000
[ 120.654429] PVR_K: (T3C-90) 0x8E05C000 0x0F08E4C0 0x0F0AD518 0x0F08B920
[ 120.654447] PVR_K: (T3C-A0) 0x0F00AEA0 0x00000000 0x00000000 0x00000000
[ 120.654465] PVR_K: (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[ 120.654484] PVR_K: (T3C-C0) 0x00000000 0x00000000 0x00000003 0x00000000
[ 120.654512] PVR_K: (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000
[ 120.654531] PVR_K: (T3C-E0) 0x0F00A420 0x0F00A740 0x0F08B000 0x0F08B000
[ 120.654550] PVR_K: (T3C-F0) 0x00000000 0x000006B1 0x000006B1 0x00000000
[ 120.654569] PVR_K: (T3C-100) 0x00000002 0x00000000 0xDCEAF420 0x00000001
[ 120.654587] PVR_K: (T3C-110) 0x00000000 0x23030000 0x33110180 0x0F0000CD
[ 120.654604] PVR_K: SGX Kernel CCB WO:0x3A RO:0x3A
[ 180.667031] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[ 180.667069] PVR_K: SGX debug (SGX_DDK_Linux_CustomerTI sgxddk 19 1.9@2188537)
[ 180.667089] PVR_K: (P0) EUR_CR_CORE_ID: 01120000
[ 180.667104] PVR_K: (P0) EUR_CR_CORE_REVISION: 00010205
[ 180.667120] PVR_K: (P0) EUR_CR_EVENT_STATUS: 00000000
[ 180.667135] PVR_K: (P0) EUR_CR_EVENT_STATUS2: 00000010
[ 180.667150] PVR_K: (P0) EUR_CR_BIF_CTRL: 00000000
[ 180.667165] PVR_K: (P0) EUR_CR_BIF_INT_STAT: 00000000
[ 180.667180] PVR_K: (P0) EUR_CR_BIF_FAULT: 00000000
[ 180.667195] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[ 180.667210] PVR_K: (P0) EUR_CR_CLKGATECTL: 00222220
[ 180.667225] PVR_K: (P0) EUR_CR_PDS_PC_BASE: 003019DC
[ 180.667246] PVR_K: Flip Command Complete Data 0 for display device 1:
[ 180.667261] PVR_K: SGX Host control:
[ 180.667278] PVR_K: (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[ 180.667296] PVR_K: (HC-10) 0x00000004 0x00000001 0x0000000A 0x00030D40
[ 180.667314] PVR_K: (HC-20) 0x00000000 0x00000001 0x00000001 0x00000000
[ 180.667333] PVR_K: (HC-30) 0x00000000 0x000279BD 0x951A1FF0 0x00000000
[ 180.667351] PVR_K: (HC-40) 0x00000000 0x00000000 0x27110194 0x0F0000E6
[ 180.667365] PVR_K: SGX TA/3D control:
[ 180.667381] PVR_K: (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[ 180.667400] PVR_K: (T3C-10) 0x00000000 0x00000000 0x00000002 0x00000000
[ 180.667418] PVR_K: (T3C-20) 0x00000000 0x00000000 0x00000000 0x00000000
[ 180.667436] PVR_K: (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[ 180.667454] PVR_K: (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[ 180.667472] PVR_K: (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[ 180.667490] PVR_K: (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[ 180.667521] PVR_K: (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[ 180.667540] PVR_K: (T3C-80) 0x00000000 0x00000000 0x0F0AD55C 0x0F000000
[ 180.667559] PVR_K: (T3C-90) 0x8E05C000 0x0F08F480 0x0F0AD55C 0x0F08B920
[ 180.667577] PVR_K: (T3C-A0) 0x0F00AEA0 0x00000000 0x00000000 0x00000000
[ 180.667595] PVR_K: (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[ 180.667613] PVR_K: (T3C-C0) 0x00000000 0x00000000 0x00000004 0x00000000
[ 180.667632] PVR_K: (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000
[ 180.667651] PVR_K: (T3C-E0) 0x0F00A420 0x0F00A740 0x0F08B000 0x0F08B000
[ 180.667669] PVR_K: (T3C-F0) 0x00000000 0x000006B1 0x000006B1 0x00000000
[ 180.667688] PVR_K: (T3C-100) 0x00000002 0x00000000 0xDCF88420 0x00000000
[ 180.667707] PVR_K: (T3C-110) 0x00000000 0x23030000 0x33110180 0x0F0000CD
[ 180.667749] PVR_K: SGX Kernel CCB WO:0x52 RO:0x52
[ 199.910769] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[ 199.910797] PVR_K: SGX debug (SGX_DDK_Linux_CustomerTI sgxddk 19 1.9@2188537)
[ 199.910817] PVR_K: (P0) EUR_CR_CORE_ID: 01120000
[ 199.910833] PVR_K: (P0) EUR_CR_CORE_REVISION: 00010205
[ 199.910848] PVR_K: (P0) EUR_CR_EVENT_STATUS: 20000000
[ 199.910864] PVR_K: (P0) EUR_CR_EVENT_STATUS2: 00000010
[ 199.910879] PVR_K: (P0) EUR_CR_BIF_CTRL: 00000000
[ 199.910894] PVR_K: (P0) EUR_CR_BIF_INT_STAT: 00000000
[ 199.910909] PVR_K: (P0) EUR_CR_BIF_FAULT: 00000000
[ 199.910924] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000002
[ 199.910939] PVR_K: (P0) EUR_CR_CLKGATECTL: 00222220
[ 199.910955] PVR_K: (P0) EUR_CR_PDS_PC_BASE: 00302034
[ 199.910978] PVR_K: Flip Command Complete Data 0 for display device 1:
[ 199.910994] PVR_K: SGX Host control:
[ 199.911011] PVR_K: (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[ 199.911029] PVR_K: (HC-10) 0x00000004 0x00000002 0x0000000A 0x00030D40
[ 199.911056] PVR_K: (HC-20) 0x00000000 0x00000000 0x00000003 0x00000000
[ 199.911075] PVR_K: (HC-30) 0x00000000 0x0002C4D8 0xB8DF88D0 0x00000000
[ 199.911094] PVR_K: (HC-40) 0x00000000 0x00000000 0x27110194 0x0F0000E6
[ 199.911108] PVR_K: SGX TA/3D control:
[ 199.911125] PVR_K: (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[ 199.911143] PVR_K: (T3C-10) 0x00000000 0x00000000 0x00000002 0x00000000
[ 199.911161] PVR_K: (T3C-20) 0x00000000 0x00000000 0x00000000 0x00000000
[ 199.911179] PVR_K: (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[ 199.911197] PVR_K: (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[ 199.911215] PVR_K: (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[ 199.911233] PVR_K: (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[ 199.911251] PVR_K: (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[ 199.911270] PVR_K: (T3C-80) 0x00000000 0x00000000 0x0F0AD518 0x0F000000
[ 199.911289] PVR_K: (T3C-90) 0x8E05C000 0x0F090440 0x0F0AD518 0x0F08B920
[ 199.911307] PVR_K: (T3C-A0) 0x0F00AEA0 0x00000000 0x00000000 0x00020000
[ 199.911325] PVR_K: (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[ 199.911344] PVR_K: (T3C-C0) 0x00000000 0x00000000 0x00000005 0x00000000
[ 199.911363] PVR_K: (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000
[ 199.911381] PVR_K: (T3C-E0) 0x0F00A420 0x0F00A740 0x0F08B000 0x0F08B000
[ 199.911400] PVR_K: (T3C-F0) 0x00000000 0x000006B1 0x000006B1 0x00000001
[ 199.911419] PVR_K: (T3C-100) 0x00000003 0x00000004 0xDCF88420 0x00000001
[ 199.911450] PVR_K: (T3C-110) 0x00000000 0x23030000 0x33110180 0x0F0000CD
[ 199.911467] PVR_K: SGX Kernel CCB WO:0x64 RO:0x56
[ 240.675869] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[ 240.675895] PVR_K: SGX debug (SGX_DDK_Linux_CustomerTI sgxddk 19 1.9@2188537)
[ 240.675914] PVR_K: (P0) EUR_CR_CORE_ID: 01120000
[ 240.675930] PVR_K: (P0) EUR_CR_CORE_REVISION: 00010205
[ 240.675945] PVR_K: (P0) EUR_CR_EVENT_STATUS: 00000000
[ 240.675960] PVR_K: (P0) EUR_CR_EVENT_STATUS2: 00000010
[ 240.675976] PVR_K: (P0) EUR_CR_BIF_CTRL: 00000000
[ 240.675990] PVR_K: (P0) EUR_CR_BIF_INT_STAT: 00000000
[ 240.676005] PVR_K: (P0) EUR_CR_BIF_FAULT: 00000000
[ 240.676020] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[ 240.676035] PVR_K: (P0) EUR_CR_CLKGATECTL: 00222220
[ 240.676073] PVR_K: (P0) EUR_CR_PDS_PC_BASE: 0030298C
[ 240.676094] PVR_K: Flip Command Complete Data 0 for display device 1:
[ 240.676111] PVR_K: SGX Host control:
[ 240.676127] PVR_K: (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[ 240.676145] PVR_K: (HC-10) 0x00000005 0x00000002 0x0000000A 0x00030D40
[ 240.676163] PVR_K: (HC-20) 0x00000000 0x00000001 0x00000001 0x00000000
[ 240.676182] PVR_K: (HC-30) 0x00000000 0x00036414 0xC457C880 0x00000000
[ 240.676200] PVR_K: (HC-40) 0x00000000 0x00000000 0x27110194 0x0F0000E6
[ 240.676214] PVR_K: SGX TA/3D control:
[ 240.676231] PVR_K: (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[ 240.676249] PVR_K: (T3C-10) 0x00000000 0x00000000 0x00000002 0x00000000
[ 240.676267] PVR_K: (T3C-20) 0x00000000 0x00000000 0x00000000 0x00000000
[ 240.676285] PVR_K: (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[ 240.676303] PVR_K: (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[ 240.676321] PVR_K: (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[ 240.676339] PVR_K: (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[ 240.676357] PVR_K: (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[ 240.676376] PVR_K: (T3C-80) 0x00000000 0x00000000 0x0F0AD55C 0x0F000000
[ 240.676394] PVR_K: (T3C-90) 0x8E05C000 0x0F091940 0x0F0AD55C 0x0F08B920
[ 240.676412] PVR_K: (T3C-A0) 0x0F00AEA0 0x00000000 0x00000000 0x00000000
[ 240.676430] PVR_K: (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[ 240.676449] PVR_K: (T3C-C0) 0x00000000 0x00000000 0x00000006 0x00000000
[ 240.676468] PVR_K: (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000
[ 240.676486] PVR_K: (T3C-E0) 0x0F00A420 0x0F00A740 0x0F08B000 0x0F08B000
[ 240.676518] PVR_K: (T3C-F0) 0x00000000 0x000006B1 0x000006B1 0x00000000
[ 240.676538] PVR_K: (T3C-100) 0x00000002 0x00000000 0xDD1A3420 0x00000000
[ 240.676557] PVR_K: (T3C-110) 0x00000000 0x23030000 0x33110180 0x0F0000CD
[ 240.676574] PVR_K: SGX Kernel CCB WO:0x9D RO:0x9D
[ 300.653007] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[ 300.653035] PVR_K: SGX debug (SGX_DDK_Linux_CustomerTI sgxddk 19 1.9@2188537)
[ 300.653055] PVR_K: (P0) EUR_CR_CORE_ID: 01120000
[ 300.653071] PVR_K: (P0) EUR_CR_CORE_REVISION: 00010205
[ 300.653086] PVR_K: (P0) EUR_CR_EVENT_STATUS: 00000000
[ 300.653101] PVR_K: (P0) EUR_CR_EVENT_STATUS2: 00000010
[ 300.653117] PVR_K: (P0) EUR_CR_BIF_CTRL: 00000000
[ 300.653132] PVR_K: (P0) EUR_CR_BIF_INT_STAT: 00000000
[ 300.653146] PVR_K: (P0) EUR_CR_BIF_FAULT: 00000000
[ 300.653161] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[ 300.653176] PVR_K: (P0) EUR_CR_CLKGATECTL: 00222220
[ 300.653192] PVR_K: (P0) EUR_CR_PDS_PC_BASE: 00300104
[ 300.653213] PVR_K: Flip Command Complete Data 0 for display device 1:
[ 300.653228] PVR_K: SGX Host control:
[ 300.653244] PVR_K: (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[ 300.653263] PVR_K: (HC-10) 0x00000006 0x00000002 0x0000000A 0x00030D40
[ 300.653281] PVR_K: (HC-20) 0x00000000 0x00000001 0x00000001 0x00000000
[ 300.653299] PVR_K: (HC-30) 0x00000000 0x00044E5C 0xDCA40750 0x00000000
[ 300.653318] PVR_K: (HC-40) 0x00000000 0x00000000 0x27110194 0x0F0000E6
[ 300.653332] PVR_K: SGX TA/3D control:
[ 300.653348] PVR_K: (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[ 300.653366] PVR_K: (T3C-10) 0x00000000 0x00000000 0x00000002 0x00000000
[ 300.653385] PVR_K: (T3C-20) 0x00000000 0x00000000 0x00000000 0x00000000
[ 300.653403] PVR_K: (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[ 300.653420] PVR_K: (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[ 300.653438] PVR_K: (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[ 300.653456] PVR_K: (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[ 300.653475] PVR_K: (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[ 300.653493] PVR_K: (T3C-80) 0x00000000 0x00000000 0x0F0AD518 0x0F000000
[ 300.653528] PVR_K: (T3C-90) 0x8E05C000 0x0F092E40 0x0F0AD518 0x0F08B920
[ 300.653546] PVR_K: (T3C-A0) 0x0F00AEA0 0x00000000 0x00000000 0x00000000
[ 300.653564] PVR_K: (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[ 300.653582] PVR_K: (T3C-C0) 0x00000000 0x00000000 0x00000007 0x00000000
[ 300.653602] PVR_K: (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000
[ 300.653620] PVR_K: (T3C-E0) 0x0F00A420 0x0F00A740 0x0F08B000 0x0F08B000
[ 300.653638] PVR_K: (T3C-F0) 0x00000000 0x000006B1 0x000006B1 0x00000000
[ 300.653658] PVR_K: (T3C-100) 0x00000002 0x00000000 0xDD315420 0x00000000
[ 300.653677] PVR_K: (T3C-110) 0x00000000 0x23030000 0x33110180 0x0F0000CD
[ 300.653693] PVR_K: SGX Kernel CCB WO:0xB6 RO:0xB6
[ 360.661139] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[ 360.661166] PVR_K: SGX debug (SGX_DDK_Linux_CustomerTI sgxddk 19 1.9@2188537)
[ 360.661186] PVR_K: (P0) EUR_CR_CORE_ID: 01120000
[ 360.661202] PVR_K: (P0) EUR_CR_CORE_REVISION: 00010205
[ 360.661217] PVR_K: (P0) EUR_CR_EVENT_STATUS: 00000000
[ 360.661233] PVR_K: (P0) EUR_CR_EVENT_STATUS2: 00000010
[ 360.661248] PVR_K: (P0) EUR_CR_BIF_CTRL: 00000000
[ 360.661262] PVR_K: (P0) EUR_CR_BIF_INT_STAT: 00000000
[ 360.661277] PVR_K: (P0) EUR_CR_BIF_FAULT: 00000000
[ 360.661303] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[ 360.661319] PVR_K: (P0) EUR_CR_CLKGATECTL: 00222220
[ 360.661334] PVR_K: (P0) EUR_CR_PDS_PC_BASE: 00300A64
[ 360.661355] PVR_K: Flip Command Complete Data 0 for display device 1:
[ 360.661370] PVR_K: SGX Host control:
[ 360.661386] PVR_K: (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[ 360.661404] PVR_K: (HC-10) 0x00000007 0x00000002 0x0000000A 0x00030D40
[ 360.661423] PVR_K: (HC-20) 0x00000000 0x00000001 0x00000001 0x00000000
[ 360.661441] PVR_K: (HC-30) 0x00000000 0x000538C3 0x0063F1F0 0x00000000
[ 360.661459] PVR_K: (HC-40) 0x00000000 0x00000000 0x27110194 0x0F0000E6
[ 360.661474] PVR_K: SGX TA/3D control:
[ 360.661490] PVR_K: (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[ 360.661518] PVR_K: (T3C-10) 0x00000000 0x00000000 0x00000002 0x00000000
[ 360.661536] PVR_K: (T3C-20) 0x00000000 0x00000000 0x00000000 0x00000000
[ 360.661554] PVR_K: (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[ 360.661573] PVR_K: (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[ 360.661590] PVR_K: (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[ 360.661609] PVR_K: (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[ 360.661627] PVR_K: (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[ 360.661645] PVR_K: (T3C-80) 0x00000000 0x00000000 0x0F0AD55C 0x0F000000
[ 360.661664] PVR_K: (T3C-90) 0x8E05C000 0x0F094340 0x0F0AD55C 0x0F08B920
[ 360.661688] PVR_K: (T3C-A0) 0x0F00AEA0 0x00000000 0x00000000 0x00000000
[ 360.661706] PVR_K: (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[ 360.661740] PVR_K: (T3C-C0) 0x00000000 0x00000000 0x00000008 0x00000000
[ 360.661760] PVR_K: (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000
[ 360.661779] PVR_K: (T3C-E0) 0x0F00A420 0x0F00A740 0x0F08B000 0x0F08B000
[ 360.661797] PVR_K: (T3C-F0) 0x00000000 0x000006B1 0x000006B1 0x00000000
[ 360.661816] PVR_K: (T3C-100) 0x00000002 0x00000000 0xDD44F420 0x00000001
[ 360.661835] PVR_K: (T3C-110) 0x00000000 0x23030000 0x33110180 0x0F0000CD
[ 360.661852] PVR_K: SGX Kernel CCB WO:0xCF RO:0xCF
[ 420.651315] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[ 420.651347] PVR_K: SGX debug (SGX_DDK_Linux_CustomerTI sgxddk 19 1.9@2188537)
[ 420.651367] PVR_K: (P0) EUR_CR_CORE_ID: 01120000
[ 420.651383] PVR_K: (P0) EUR_CR_CORE_REVISION: 00010205
[ 420.651398] PVR_K: (P0) EUR_CR_EVENT_STATUS: 00000000
[ 420.651413] PVR_K: (P0) EUR_CR_EVENT_STATUS2: 00000010
[ 420.651429] PVR_K: (P0) EUR_CR_BIF_CTRL: 00000000
[ 420.651444] PVR_K: (P0) EUR_CR_BIF_INT_STAT: 00000000
[ 420.651458] PVR_K: (P0) EUR_CR_BIF_FAULT: 00000000
[ 420.651473] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[ 420.651489] PVR_K: (P0) EUR_CR_CLKGATECTL: 00222220
[ 420.651533] PVR_K: (P0) EUR_CR_PDS_PC_BASE: 003013B4
[ 420.651555] PVR_K: Flip Command Complete Data 0 for display device 1:
[ 420.651570] PVR_K: SGX Host control:
[ 420.651598] PVR_K: (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[ 420.651616] PVR_K: (HC-10) 0x00000008 0x00000002 0x0000000A 0x00030D40
[ 420.651634] PVR_K: (HC-20) 0x00000000 0x00000001 0x00000001 0x00000000
[ 420.651653] PVR_K: (HC-30) 0x00000000 0x00062318 0x24287070 0x00000000
[ 420.651671] PVR_K: (HC-40) 0x00000000 0x00000000 0x27110194 0x0F0000E6
[ 420.651686] PVR_K: SGX TA/3D control:
[ 420.651702] PVR_K: (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[ 420.651745] PVR_K: (T3C-10) 0x00000000 0x00000000 0x00000002 0x00000000
[ 420.651764] PVR_K: (T3C-20) 0x00000000 0x00000000 0x00000000 0x00000000
[ 420.651782] PVR_K: (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[ 420.651800] PVR_K: (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[ 420.651818] PVR_K: (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[ 420.651836] PVR_K: (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[ 420.651854] PVR_K: (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[ 420.651872] PVR_K: (T3C-80) 0x00000000 0x00000000 0x0F0AD518 0x0F000000
[ 420.651898] PVR_K: (T3C-90) 0x8E05C000 0x0F095840 0x0F0AD518 0x0F08B920
[ 420.651916] PVR_K: (T3C-A0) 0x0F00AEA0 0x00000000 0x00000000 0x00000000
[ 420.651934] PVR_K: (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[ 420.651952] PVR_K: (T3C-C0) 0x00000000 0x00000000 0x00000009 0x00000000
[ 420.651971] PVR_K: (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000
[ 420.651990] PVR_K: (T3C-E0) 0x0F00A420 0x0F00A740 0x0F08B000 0x0F08B000
[ 420.652008] PVR_K: (T3C-F0) 0x00000000 0x000006B1 0x000006B1 0x00000000
[ 420.652027] PVR_K: (T3C-100) 0x00000002 0x00000000 0xDD581420 0x00000002
[ 420.652047] PVR_K: (T3C-110) 0x00000000 0x23030000 0x33110180 0x0F0000CD
[ 420.652063] PVR_K: SGX Kernel CCB WO:0xD5 RO:0xD5
[ 480.669530] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[ 480.669557] PVR_K: SGX debug (SGX_DDK_Linux_CustomerTI sgxddk 19 1.9@2188537)
[ 480.669578] PVR_K: (P0) EUR_CR_CORE_ID: 01120000
[ 480.669594] PVR_K: (P0) EUR_CR_CORE_REVISION: 00010205
[ 480.669609] PVR_K: (P0) EUR_CR_EVENT_STATUS: 00000000
[ 480.669624] PVR_K: (P0) EUR_CR_EVENT_STATUS2: 00000010
[ 480.669639] PVR_K: (P0) EUR_CR_BIF_CTRL: 00000000
[ 480.669654] PVR_K: (P0) EUR_CR_BIF_INT_STAT: 00000000
[ 480.669669] PVR_K: (P0) EUR_CR_BIF_FAULT: 00000000
[ 480.669684] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[ 480.669699] PVR_K: (P0) EUR_CR_CLKGATECTL: 00222220
[ 480.669738] PVR_K: (P0) EUR_CR_PDS_PC_BASE: 00301D04
[ 480.669760] PVR_K: Flip Command Complete Data 0 for display device 1:
[ 480.669775] PVR_K: SGX Host control:
[ 480.669791] PVR_K: (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[ 480.669810] PVR_K: (HC-10) 0x00000009 0x00000002 0x0000000A 0x00030D40
[ 480.669828] PVR_K: (HC-20) 0x00000000 0x00000001 0x00000001 0x00000000
[ 480.669846] PVR_K: (HC-30) 0x00000000 0x00070D89 0x47EA2FD0 0x00000000
[ 480.669865] PVR_K: (HC-40) 0x00000000 0x00000000 0x27110194 0x0F0000E6
[ 480.669880] PVR_K: SGX TA/3D control:
[ 480.669896] PVR_K: (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[ 480.669914] PVR_K: (T3C-10) 0x00000000 0x00000000 0x00000002 0x00000000
[ 480.669932] PVR_K: (T3C-20) 0x00000000 0x00000000 0x00000000 0x00000000
[ 480.669950] PVR_K: (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[ 480.669968] PVR_K: (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[ 480.669986] PVR_K: (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[ 480.670004] PVR_K: (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[ 480.670022] PVR_K: (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[ 480.670041] PVR_K: (T3C-80) 0x00000000 0x00000000 0x0F0AD55C 0x0F000000
[ 480.670059] PVR_K: (T3C-90) 0x8E05C000 0x0F096D40 0x0F0AD55C 0x0F08B920
[ 480.670078] PVR_K: (T3C-A0) 0x0F00AEA0 0x00000000 0x00000000 0x00000000
[ 480.670095] PVR_K: (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[ 480.670113] PVR_K: (T3C-C0) 0x00000000 0x00000000 0x0000000A 0x00000000
[ 480.670133] PVR_K: (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000
[ 480.670151] PVR_K: (T3C-E0) 0x0F00A420 0x0F00A740 0x0F08B000 0x0F08B000
[ 480.670169] PVR_K: (T3C-F0) 0x00000000 0x000006B1 0x000006B1 0x00000000
[ 480.670188] PVR_K: (T3C-100) 0x00000002 0x00000000 0xDD6FB420 0x00000001
[ 480.670208] PVR_K: (T3C-110) 0x00000000 0x23030000 0x33110180 0x0F0000CD
[ 480.670224] PVR_K: SGX Kernel CCB WO:0xED RO:0xED
[ 540.657654] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[ 540.657682] PVR_K: SGX debug (SGX_DDK_Linux_CustomerTI sgxddk 19 1.9@2188537)
[ 540.657702] PVR_K: (P0) EUR_CR_CORE_ID: 01120000
[ 540.657742] PVR_K: (P0) EUR_CR_CORE_REVISION: 00010205
[ 540.657758] PVR_K: (P0) EUR_CR_EVENT_STATUS: 00000000
[ 540.657773] PVR_K: (P0) EUR_CR_EVENT_STATUS2: 00000010
[ 540.657788] PVR_K: (P0) EUR_CR_BIF_CTRL: 00000000
[ 540.657803] PVR_K: (P0) EUR_CR_BIF_INT_STAT: 00000000
[ 540.657818] PVR_K: (P0) EUR_CR_BIF_FAULT: 00000000
[ 540.657833] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[ 540.657849] PVR_K: (P0) EUR_CR_CLKGATECTL: 00222220
[ 540.657863] PVR_K: (P0) EUR_CR_PDS_PC_BASE: 0030264C
[ 540.657884] PVR_K: Flip Command Complete Data 0 for display device 1:
[ 540.657900] PVR_K: SGX Host control:
[ 540.657916] PVR_K: (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[ 540.657934] PVR_K: (HC-10) 0x0000000A 0x00000002 0x0000000A 0x00030D40
[ 540.657952] PVR_K: (HC-20) 0x00000000 0x00000001 0x00000001 0x00000000
[ 540.657981] PVR_K: (HC-30) 0x00000000 0x0007F7DC 0x6BB034F0 0x00000000
[ 540.658000] PVR_K: (HC-40) 0x00000000 0x00000000 0x27110194 0x0F0000E6
[ 540.658014] PVR_K: SGX TA/3D control:
[ 540.658031] PVR_K: (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[ 540.658049] PVR_K: (T3C-10) 0x00000000 0x00000000 0x00000002 0x00000000
[ 540.658067] PVR_K: (T3C-20) 0x00000000 0x00000000 0x00000000 0x00000000
[ 540.658085] PVR_K: (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[ 540.658103] PVR_K: (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[ 540.658121] PVR_K: (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[ 540.658139] PVR_K: (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[ 540.658157] PVR_K: (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[ 540.658186] PVR_K: (T3C-80) 0x00000000 0x00000000 0x0F0AD518 0x0F000000
[ 540.658204] PVR_K: (T3C-90) 0x8E05C000 0x0F097D00 0x0F0AD518 0x0F08B920
[ 540.658222] PVR_K: (T3C-A0) 0x0F00AEA0 0x00000000 0x00000000 0x00000000
[ 540.658241] PVR_K: (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[ 540.658259] PVR_K: (T3C-C0) 0x00000000 0x00000000 0x0000000B 0x00000000
[ 540.658277] PVR_K: (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000
[ 540.658296] PVR_K: (T3C-E0) 0x0F00A420 0x0F00A740 0x0F08B000 0x0F08B000
[ 540.658315] PVR_K: (T3C-F0) 0x00000000 0x000006B1 0x000006B1 0x00000000
[ 540.658333] PVR_K: (T3C-100) 0x00000002 0x00000000 0xDD836420 0x00000001
[ 540.658352] PVR_K: (T3C-110) 0x00000000 0x23030000 0x33110180 0x0F0000CD
[ 540.658368] PVR_K: SGX Kernel CCB WO:0xF2 RO:0xF2
[ 600.657797] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[ 600.657839] PVR_K: SGX debug (SGX_DDK_Linux_CustomerTI sgxddk 19 1.9@2188537)
[ 600.657858] PVR_K: (P0) EUR_CR_CORE_ID: 01120000
[ 600.657874] PVR_K: (P0) EUR_CR_CORE_REVISION: 00010205
[ 600.657889] PVR_K: (P0) EUR_CR_EVENT_STATUS: 00000000
[ 600.657905] PVR_K: (P0) EUR_CR_EVENT_STATUS2: 00000010
[ 600.657920] PVR_K: (P0) EUR_CR_BIF_CTRL: 00000000
[ 600.657935] PVR_K: (P0) EUR_CR_BIF_INT_STAT: 00000000
[ 600.657949] PVR_K: (P0) EUR_CR_BIF_FAULT: 00000000
[ 600.657965] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[ 600.657980] PVR_K: (P0) EUR_CR_CLKGATECTL: 00222220
[ 600.657996] PVR_K: (P0) EUR_CR_PDS_PC_BASE: 00302F94
[ 600.658016] PVR_K: Flip Command Complete Data 0 for display device 1:
[ 600.658032] PVR_K: SGX Host control:
[ 600.658049] PVR_K: (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[ 600.658067] PVR_K: (HC-10) 0x0000000B 0x00000002 0x0000000A 0x00030D40
[ 600.658085] PVR_K: (HC-20) 0x00000000 0x00000001 0x00000001 0x00000000
[ 600.658103] PVR_K: (HC-30) 0x00000000 0x0008E23B 0x8F71A630 0x00000000
[ 600.658122] PVR_K: (HC-40) 0x00000000 0x00000000 0x27110194 0x0F0000E6
[ 600.658136] PVR_K: SGX TA/3D control:
[ 600.658152] PVR_K: (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[ 600.658181] PVR_K: (T3C-10) 0x00000000 0x00000000 0x00000002 0x00000000
[ 600.658200] PVR_K: (T3C-20) 0x00000000 0x00000000 0x00000000 0x00000000
[ 600.658218] PVR_K: (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[ 600.658236] PVR_K: (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[ 600.658254] PVR_K: (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[ 600.658272] PVR_K: (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[ 600.658290] PVR_K: (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[ 600.658308] PVR_K: (T3C-80) 0x00000000 0x00000000 0x0F0AD55C 0x0F000000
[ 600.658327] PVR_K: (T3C-90) 0x8E05C000 0x0F098CC0 0x0F0AD55C 0x0F08B920
[ 600.658345] PVR_K: (T3C-A0) 0x0F00AEA0 0x00000000 0x00000000 0x00000000
[ 600.658363] PVR_K: (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[ 600.658381] PVR_K: (T3C-C0) 0x00000000 0x00000000 0x0000000C 0x00000000
[ 600.658400] PVR_K: (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000
[ 600.658419] PVR_K: (T3C-E0) 0x0F00A420 0x0F00A740 0x0F08B000 0x0F08B000
[ 600.658437] PVR_K: (T3C-F0) 0x00000000 0x000006B1 0x000006B1 0x00000000
[ 600.658456] PVR_K: (T3C-100) 0x00000002 0x00000000 0xDD971420 0x00000001
[ 600.658475] PVR_K: (T3C-110) 0x00000000 0x23030000 0x33110180 0x0F0000CD
[ 600.658491] PVR_K: SGX Kernel CCB WO:0xF7 RO:0xF7
[ 660.657929] PVR_K: HWRecoveryResetSGX: SGX Hardware Recovery triggered
[ 660.657958] PVR_K: SGX debug (SGX_DDK_Linux_CustomerTI sgxddk 19 1.9@2188537)
[ 660.657977] PVR_K: (P0) EUR_CR_CORE_ID: 01120000
[ 660.657993] PVR_K: (P0) EUR_CR_CORE_REVISION: 00010205
[ 660.658008] PVR_K: (P0) EUR_CR_EVENT_STATUS: 00000000
[ 660.658023] PVR_K: (P0) EUR_CR_EVENT_STATUS2: 00000010
[ 660.658039] PVR_K: (P0) EUR_CR_BIF_CTRL: 00000000
[ 660.658054] PVR_K: (P0) EUR_CR_BIF_INT_STAT: 00000000
[ 660.658068] PVR_K: (P0) EUR_CR_BIF_FAULT: 00000000
[ 660.658083] PVR_K: (P0) EUR_CR_BIF_MEM_REQ_STAT: 00000000
[ 660.658098] PVR_K: (P0) EUR_CR_CLKGATECTL: 00222220
[ 660.658114] PVR_K: (P0) EUR_CR_PDS_PC_BASE: 003006E4
[ 660.658134] PVR_K: Flip Command Complete Data 0 for display device 1:
[ 660.658160] PVR_K: SGX Host control:
[ 660.658187] PVR_K: (HC-0) 0x00000001 0x00000000 0x00000000 0x00000001
[ 660.658205] PVR_K: (HC-10) 0x0000000C 0x00000002 0x0000000A 0x00030D40
[ 660.658223] PVR_K: (HC-20) 0x00000000 0x00000001 0x00000001 0x00000000
[ 660.658242] PVR_K: (HC-30) 0x00000000 0x0009CC9A 0xB334EC30 0x00000000
[ 660.658261] PVR_K: (HC-40) 0x00000000 0x00000000 0x27110194 0x0F0000E6
[ 660.658275] PVR_K: SGX TA/3D control:
[ 660.658298] PVR_K: (T3C-0) 0x0F003000 0x0F003120 0x0F002000 0x00000000
[ 660.658317] PVR_K: (T3C-10) 0x00000000 0x00000000 0x00000002 0x00000000
[ 660.658335] PVR_K: (T3C-20) 0x00000000 0x00000000 0x00000000 0x00000000
[ 660.658352] PVR_K: (T3C-30) 0x00000000 0x00000000 0x00000000 0x00000000
[ 660.658370] PVR_K: (T3C-40) 0x00000000 0x00000000 0x00000000 0x00000000
[ 660.658389] PVR_K: (T3C-50) 0x00000000 0x00000000 0x00000000 0x00000000
[ 660.658406] PVR_K: (T3C-60) 0x00000000 0x00000000 0x00000000 0x00000000
[ 660.658424] PVR_K: (T3C-70) 0x00000000 0x00000000 0x00000000 0x00000000
[ 660.658443] PVR_K: (T3C-80) 0x00000000 0x00000000 0x0F0AD518 0x0F000000
[ 660.658462] PVR_K: (T3C-90) 0x8E05C000 0x0F099C80 0x0F0AD518 0x0F08B920
[ 660.658479] PVR_K: (T3C-A0) 0x0F00AEA0 0x00000000 0x00000000 0x00000000
[ 660.658497] PVR_K: (T3C-B0) 0x00000000 0x00000000 0x00000000 0x00000000
[ 660.658523] PVR_K: (T3C-C0) 0x00000000 0x00000000 0x0000000D 0x00000000
[ 660.658550] PVR_K: (T3C-D0) 0x0F000000 0x8000B000 0x8004B000 0x0F004000
[ 660.658568] PVR_K: (T3C-E0) 0x0F00A420 0x0F00A740 0x0F08B000 0x0F08B000
[ 660.658587] PVR_K: (T3C-F0) 0x00000000 0x000006B1 0x000006B1 0x00000000
[ 660.658606] PVR_K: (T3C-100) 0x00000002 0x00000000 0xDDAAC420 0x00000001
[ 660.658625] PVR_K: (T3C-110) 0x00000000 0x23030000 0x33110180 0x0F0000CD
[ 660.658641] PVR_K: SGX Kernel CCB WO:0xFC RO:0xFC

Please let me know how to resolve this problem.

  • Which version of processor SDK are you using? Is it possible to run that QT application on our processor SDK and see the behavior?

    It may be possible that source of the problem is something else manifesting into SGX issues and causing it to prints lot of PVR prints. Tell us what is special about this QT application. Also, share entire error logs that might give hint if something else ran into trouble before. 

    Also check if this thread is relevant to your issue -