This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux kernel version of AM3517EVM and bundled CD

My customer claims why the version of the Linux kernel on AM3517EVM(NAND) is differ from that on the bundled CD?

Each kernel version is;     AM3517EVM : 2-6.32-rc5

                                              Bundled CD:  2.6.31-rc7-omap1-06331-g75
 

Thanks,

KIMIZUKA

 

  • It is just a matter of when the NAND was programmed vs. when the CD was burned.  The image on the NAND is really just intended to provide an out of the box demo.

    Regards,

    James

  • Thank you for your explanation.

    As for the image on the NAND, which SDK version and tool chain are applied to build it ?

    If these environments are differ ffrom those in the bundled CD, it is not possible to re-build the exact same one with the image in the NAND.

    Is there any save and restore utility for NAND contents, in order to keep the image in the NAND ?

    Thanks and Regards,

    KIMIZUKA