Part Number: AM3352
Tool/software: Linux
Hi,
We are using a custom board based on AM3352. In NAND(Micron MT29F4G08ABADAH4)interface, our customer want to configure the NAND timing mode to 5. I think by default it is configured to timing mode 0.
1) In which place I need to configure the NAND timing mode in kernel.
2) Is timing mode can be configured through dts.?
I'm using processor-sdk-04.01.00.06 version
Regards,
Manoj