This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3358: SD card EXT4 error

Part Number: AM3358

Tool/software: Linux

Hello,

I would like to ask you for advice about system configuration running from SD card. I'm using kernel from TI 4.9.59. And due to need of our own filesystem I chose to use Buildroot. I know the TI mainly supports Yocto, but I believe someone could help me anyway.

There is the thing. The compilation is OK, I create SD card as recomended by buildroot by: dd if=${BASEDIR}/../output/images/sdcard.img of=/dev/mmcblk0. It creates two partitions on the SD. The Linux boots OKish but after while wierd Ext-4 errors appear. Here is some example I got.

[ 17.243011] EXT4-fs error (device mmcblk0p2) in ext4_reserve_inode_write:5434: Out y
[ 17.256024] EXT4-fs error (device mmcblk0p2) in ext4_orphan_add:2845: Out of memory
[ 17.268580] EXT4-fs error (device mmcblk0p2) in ext4_reserve_inode_write:5434: Out of memory
[ 17.280781] EXT4-fs error (device mmcblk0p2) in ext4_setattr:5261: Out of memory
[ 19.682658] EXT4-fs error (device mmcblk0p2): ext4_map_blocks:567: inode #8: block 114770: comm jbd2)
[ 19.700038] jbd2_journal_bmap: journal block not found at offset 81 on mmcblk0p2-8
[ 19.709030] Aborting journal on device mmcblk0p2-8.
[ 37.046792] EXT4-fs error (device mmcblk0p2): ext4_journal_check_start:56: Detected aborted journal
[ 37.056102] EXT4-fs (mmcblk0p2): Remounting filesystem read-only
[ 37.067945] EXT4-fs (mmcblk0p2): ext4_writepages: jbd2_start: 3072 pages, ino 4342; err -30
[ 60.772476] random: crng init done
[ 305.122423] EXT4-fs (mmcblk0p2): error count since last fsck: 39
[ 305.128516] EXT4-fs (mmcblk0p2): initial error at time 65536:
�:0: inode 8: block 524288
[ 305.136965] EXT4-fs (mmcblk0p2): last error at time 1513289431: ext4_journal_check_start:56: inode 80

Eventually it leads to total kernel panic. I tried multiple SD cards, same behavior. I switched the journald to use volatile memory, but I'm definitely missing something.

Below is attaged my Buildroot defconfig.

Any help would be appreciated.

BR2_arm=y
BR2_cortex_a8=y
BR2_CCACHE=y
BR2_GLOBAL_PATCH_DIR="board/prusa/einsy_pro/patches"
BR2_TOOLCHAIN_EXTERNAL=y
BR2_TARGET_GENERIC_HOSTNAME="prusa_pro"
BR2_TARGET_GENERIC_ISSUE="Welcome to Prusa"
BR2_INIT_SYSTEMD=y
BR2_TARGET_GENERIC_ROOT_PASSWD="toor"
BR2_SYSTEM_BIN_SH_BASH=y
BR2_TARGET_GENERIC_GETTY_PORT="ttyO0"
BR2_ROOTFS_OVERLAY="board/prusa/einsy_pro/rootfs_overlay"
BR2_ROOTFS_POST_IMAGE_SCRIPT="board/prusa/einsy_pro/post-image.sh"
BR2_LINUX_KERNEL=y
BR2_LINUX_KERNEL_CUSTOM_GIT=y
BR2_LINUX_KERNEL_CUSTOM_REPO_URL="https://github.com/filipkotoucek/tisdk_linux.git"
BR2_LINUX_KERNEL_CUSTOM_REPO_VERSION="development"
BR2_LINUX_KERNEL_USE_CUSTOM_CONFIG=y
BR2_LINUX_KERNEL_CUSTOM_CONFIG_FILE="board/prusa/einsy_pro/linux_defconfig"
BR2_LINUX_KERNEL_DTS_SUPPORT=y
BR2_LINUX_KERNEL_INTREE_DTS_NAME="am335x-bone am335x-boneblack am335x-prusa-pro"
BR2_PACKAGE_BUSYBOX_CONFIG="board/prusa/einsy_pro/busybox.config"
BR2_PACKAGE_SPIDEV_TEST=y
BR2_PACKAGE_PYTHON=y
BR2_PACKAGE_PYTHON_SPIDEV=y
BR2_PACKAGE_DTC=y
BR2_PACKAGE_DTC_PROGRAMS=y
BR2_PACKAGE_DROPBEAR=y
BR2_PACKAGE_VIM=y
BR2_TARGET_ROOTFS_EXT2=y
BR2_TARGET_ROOTFS_EXT2_4=y
BR2_TARGET_ROOTFS_EXT2_SIZE="256M"
BR2_TARGET_UBOOT=y
BR2_TARGET_UBOOT_BUILD_SYSTEM_KCONFIG=y
BR2_TARGET_UBOOT_CUSTOM_VERSION=y
BR2_TARGET_UBOOT_CUSTOM_VERSION_VALUE="2017.01"
BR2_TARGET_UBOOT_BOARD_DEFCONFIG="am335x_boneblack"
BR2_TARGET_UBOOT_NEEDS_DTC=y
# BR2_TARGET_UBOOT_FORMAT_BIN is not set
BR2_TARGET_UBOOT_FORMAT_IMG=y
BR2_TARGET_UBOOT_FORMAT_CUSTOM=y
BR2_TARGET_UBOOT_FORMAT_CUSTOM_NAME="spl/u-boot-spl.bin"
BR2_TARGET_UBOOT_SPL=y
BR2_TARGET_UBOOT_SPL_NAME="MLO"
BR2_PACKAGE_HOST_DOSFSTOOLS=y
BR2_PACKAGE_HOST_GENIMAGE=y
BR2_PACKAGE_HOST_MTOOLS=y

  • Hi,

    Current Linux Processor SDK release is based on kernel v4.9.41. Other releases or Linux versions are not supported on this forum.
  • The TI SDK 04.02.00.09 includes kernel 4.9.59 which I am using.
  • Sorry, my mistake there. I have notified the software team. They will respond here.
  • Hello Filip,

    There are remains from your previous formatting which confuses the ext4 filesystem. Please overwrite the complete data on your SD card with zeroes before flashing your new image.

    dd if=/dev/zero of=/dev/sdX

    Best regards,
    Kemal
  • I already did that but nothing changed.

    When I tried to DD card again and write the image into it, I got these errors after boot:

    [ 18.422901] EXT4-fs error (device mmcblk0p2): mb_free_blocks:1470: group 1, block 33283:freeing already freed block (bit 515); block bitmap corrupt.
    [ 18.436628] EXT4-fs error (device mmcblk0p2): ext4_mb_generate_buddy:758: group 1, block bitmap and bg descriptor inconsistent: 30010 vs 30011 free clusters

    After next reboot I got the error messages when the device is booting up:

    [ 1.731485] ALSA device list:
    [ 1.734557] No soundcards found.
    [ 1.750369] EXT4-fs (mmcblk0p2): warning: mounting fs with errors, running e2fsck is recommended
    [ 1.763438] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    [ 1.771630] VFS: Mounted root (ext4 filesystem) on device 179:2.
    [ 1.779902] devtmpfs: mounted
    [ 1.784394] Freeing unused kernel memory: 1024K
    ...
    [ OK ] Reached target Local File Systems.
    Starting Rebuild Journal Catalog...
    [ 3.953640] systemd-journald[89]: Received request to flush runtime journal from PID 1
    [ 4.020297] EXT4-fs error (device mmcblk0p2): ext4_mb_generate_buddy:758: group 1, block bitmap and bg descriptor inconsistent: 30517 vs 30518 free clusters
    [ OK ] Started Flush Journal to Persistent Storage.
    Starting Create Volatile Files and Directories...
    [ 4.094186] JBD2: Spotted dirty metadata buffer (dev = mmcblk0p2, blocknr = 0). There's a risk of filesystem corruption in case of system crash.
    [ OK ] Started Rebuild Journal Catalog.

    Could it be caused by some bad allocation? When I write the image to 8 GB SD card it creates two partitions:

    /dev/mmcblk0p1 16MB first sector 1, last sector 32768, flasgs boot lba
    /dev/mmcblk0p2 512MB first sector 32769, last sector 1081344
    unalocated first sector 1081345, last sector 15759359

    Or does the linux writes something many times somewhere into SD card so it causes the damaged sector?
    I have the second partition mounted via USB gadget driver as mass storage. So could it be caused by improper device handling?
  • We need to narrow down the issue to understand why this happens. Can you boot with the kernel from the latest Processor SDK since this issue can be seen only with bildroot's kernel? Can you attach that SD card to your host machine or tftpboot and run e2fsck on that mmcblk0p2 partition? If there is no success, can you copy the rootfs files with cp -rp to another location then mkfs.ext4 that partition and copy the files back?

  • It seems the problem is in mounting mmblck0p2 over g_multi driver. When I switch to using just g_ether without sharing the filesystem from SD card it seems it is working. I send the configuration and shell scripts handling g_multi.

    #!/bin/sh
    
    # Based off:
    # https://github.com/RobertCNelson/boot-scripts/blob/master/boot/am335x_evm.sh
    
    # Assume some defaults
    SERIAL_NUMBER="1234BBBK5678"
    PRODUCT="am335x_evm"
    manufacturer="ti.com"
    
    # Read serial numberfrom the eerpom
    eeprom="/sys/bus/i2c/devices/0-0050/eeprom"
    if [ -f ${eeprom} ] ; then
    	SERIAL_NUMBER=$(hexdump -e '8/1 "%c"' ${eeprom} -n 28 | cut -b 17-28)
    	PRODUCT="BeagleBoneBlack"
    	manufacturer="BeagleBoard.org"
    fi
    
    echo "SERIAL_NUMBER = ${SERIAL_NUMBER}"
    echo "PRODUCT = ${PRODUCT}"
    
    #save location of MAC address, otherwise exit
    mac_address="/proc/device-tree/ocp/ethernet@4a100000/slave@4a100300/mac-address"
    [ -r "$mac_address" ] || exit 0
    
    #save MAC address as address of this device
    dev_addr=$(/usr/bin/hexdump -v -e '5/1 "%02X:" 1/1 "%02X"' "$mac_address")
    echo "dev_addr = ${dev_addr}"
    
    #define static MAC for host PC. Swap last digit to 0
    host_addr="${dev_addr:0:-1}0"
    echo "host_addr = ${host_addr}"
    
    # Set the g_multi parameters (read-write, removable)
    g_defaults="cdrom=0 ro=0 stall=0 removable=1 nofua=1"
    g_product="iSerialNumber=${SERIAL_NUMBER} iManufacturer=${manufacturer} iProduct=${PRODUCT}"
    g_network="dev_addr=${dev_addr} host_addr=${host_addr}"
    g_storage="file=/dev/mmcblk0p2"
    
    #start g_multi module. It starts usb0 interface and mounts rootfs as removable device
    modprobe g_multi ${g_storage} ${g_defaults} ${g_product} ${g_network}
    #modprobe g_ether ${g_network}
    
    # Bring up the USB network interface
    ifdown usb0
    ifup usb0
    

    [Unit]
    Description=Start USB gadget
    Requires=dev-mmcblk0p2.device
    #Wants=serial-getty@ttyS0.service
    Wants=udhcpd.service
    
    After=dev-mmcblk0p2.device
    #Before=serial-getty@ttyS0.service
    Before=udhcpd.service
    
    [Service]
    Type=oneshot
    RemainAfterExit=yes
    ExecStart=/usr/bin/usb-ethernet.sh
    #ExecStopPre=/bin/systemctl stop serial-getty@ttyGS0.service
    ExecStop=/sbin/rmmod g_multi
    
    [Install]
    WantedBy=basic.target
    
    

  • Yes, it is possible to be caused by g_multi driver. I am sending you the scripts from the latest Processor SDK.

    #!/bin/sh
    
    # Based off:
    # https://github.com/RobertCNelson/boot-scripts/blob/master/boot/am335x_evm.sh
    
    # Assume some defaults
    SERIAL_NUMBER="1234BBBK5678"
    PRODUCT="am335x_evm"
    manufacturer="ti.com"
    
    # Read serial numberfrom the eerpom
    eeprom="/sys/bus/i2c/devices/0-0050/eeprom"
    if [ -f ${eeprom} ] ; then
        SERIAL_NUMBER=$(hexdump -e '8/1 "%c"' ${eeprom} -n 28 | cut -b 17-28)
        PRODUCT="BeagleBoneBlack"
        manufacturer="BeagleBoard.org"
    fi
    
    echo "SERIAL_NUMBER = ${SERIAL_NUMBER}"
    echo "PRODUCT = ${PRODUCT}"
    
    
    mac_address="/proc/device-tree/ocp/ethernet@4a100000/slave@4a100300/mac-address"
    [ -r "$mac_address" ] || exit 0
    
    host_addr=$(/usr/bin/hexdump -v -e '5/1 "%02X:" 1/1 "%02X"' "$mac_address")
    echo "host_addr = ${host_addr}"
    
    # Set the g_multi parameters
    g_defaults="cdrom=0 ro=1 stall=0 removable=1 nofua=1"
    
    g_product="iSerialNumber=${SERIAL_NUMBER} iManufacturer=${manufacturer} iProduct=${PRODUCT}"
    
    g_network="host_addr=${host_addr}"
    
    g_storage="file=/dev/mmcblk0p1"
    
    modprobe g_multi ${g_storage} ${g_defaults} ${g_product} ${g_network}
    
    # Bring up the USB network interface
    ifup usb0
    

    [Unit]
    Description=Start USB gadget
    Requires=dev-mmcblk0p1.device
    Wants=serial-getty@ttyGS0.service
    Wants=busybox-udhcp.service
    
    After=dev-mmcblk0p1.device
    Before=serial-getty@ttyGS0.service
    Before=busybox-udhcp.service
    
    [Service]
    Type=oneshot
    RemainAfterExit=yes
    ExecStart=/usr/bin/gadget-init.sh
    ExecStopPre=/bin/systemctl stop serial-getty@ttyGS0.service
    ExecStop=/sbin/rmmod g_multi
    
    [Install]
    WantedBy=basic.target