Hi Sitara Team,
My customer needs to accommodate for a high noise environment, but is having some issues understanding how to take the ADC driver provided by us and do oversampling, front-end digital filtering, and controlling the sample rate and sample periods to using the ADC on our AM3352 running Lynx.
To us it seems that the Sitara ADC Lynx driver options are either a single shot or a continuous read mode. In continuous read mode, their F/W team confirms if the ADC output file is not read in time the data output file overflows. In single shot, the Lynx can gather 1 value every 10ms, and what the EVSE system provide can vary 2 to 1 in Voltage measured.
They are asking for help with these drivers in order to harden against the severe noise seen during EV charging. Can we possibly provide them with information on what F/W enhancements can be added at the driver level, that will help their Lynx embedded solutions?
Thanks!
Barend