This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: MMC_CMD delay through IODELAY

Part Number: AM5728

I need to integrate a sdio 3.3V high speed wifi Board with AM5728 board.

But the sdio wifi have a bug, the response on cmd line change in rising edge. So in cmd input direction, I can see real input hold time about 2.5ns which expected to be 5ns.

The sdio wifi vendor need me add resistor in cmd line, but it's hard for my AM5728 board.

Can you use IODELAY in mmc1 cmd input , to delay cmd >2.5ns ?

I read posts in the forum, saying need to get PCT?

Can experts here provide me a max A_delay G_delay value for trying?