Part Number: TDA3MV
Hi,
I would like to confirm about IOSET of QSPI and the AC timing.
It is described in TDA 3 MV data sheet 7.13 Quad Serial Peripheral Interface (QSPI) as follows.
-------------------
CAUTION
The IO timings provided in this section are only valid if signals within a single IOSET are used. The IOSETs are defined in Table 7-25.
-------------------
When I select the following ball with QSPI (ball selection combining IOSET), please let me know how the TDA3x's QSPI peripheral will behave.
qspi1_sclk:C8
qspi1_rtclk:C14
qspi1_d0:B9
qspi1_d1:F10
qspi1_d2:A9
qspi1_d3:D10
qspi1_cs0:E10
qspi1_cs1:F15
In this case, Is Clock Mode 0 unusable (can not use Rtclk)?
QSPI AC timing can not be satisfied?
What is the specification when the timing is not satisfied?
Regards,
Kenshow