Part Number: PROCESSOR-SDK-AM335X
every expecter
This is Tomiyama From Tokyo.
Thanks a lot of helps.
I have connect to PC sucssesfuly. but I just use a Startware without modify.
When I try to modify the source code, there are errors bellow.
I could not know who use the 0x8000,0000 memory.
could you help me ?
I need your help as soon as posiable.
best regards
Tomiyama.
usb_dev_serial.cmd:
MEMORY
{
DDR_MEM : org = 0x80000000 len = 0x7FFFFFF /* RAM */
}
error log:
**** Clean-only build of configuration Debug for project usb_dev_serial ****
"C:\\ti\\ccsv7\\utils\\bin\\gmake" -k -j 4 -s clean -O
'Finished clean'
' '
**** Build Finished ****
**** Build of configuration Debug for project usb_dev_serial ****
"C:\\ti\\ccsv7\\utils\\bin\\gmake" -k -j 4 -s all -O
'Building file: C:/New Folder/examples/evmskAM335x/usb_dev_serial/usb_serial_structs.c'
'Invoking: ARM Compiler'
'Finished building: C:/New Folder/examples/evmskAM335x/usb_dev_serial/usb_serial_structs.c'
' '
'Building file: C:/New Folder/examples/evmskAM335x/usb_dev_serial/ustdlib.c'
'Invoking: ARM Compiler'
'Finished building: C:/New Folder/examples/evmskAM335x/usb_dev_serial/ustdlib.c'
' '
'Building file: C:/New Folder/examples/evmskAM335x/usb_dev_serial/Usb_dev_serial.c'
'Invoking: ARM Compiler'
"../../../../../../../include/hw/hw_lcdc.h", line 107: warning #1557-D: white space between backslash and newline in line splice ignored
'Finished building: C:/New Folder/examples/evmskAM335x/usb_dev_serial/Usb_dev_serial.c'
' '
'Building target: ../../../../../../../binary/armv7a/cgt_ccs/am335x/evmskAM335x/usb_dev_serial/usb_dev_serial.out'
'Invoking: ARM Linker'
< Linking>
"../usb_dev_serial.cmd", line 78: error #10263: DDR_MEM memory range has
already been specified
"../usb_dev_serial.cmd", line 78: error #10264: DDR_MEM memory range overlaps
existing memory range DDR_MEM
"../usb_dev_serial.cmd", line 92: warning #10190-D: absolute symbol "bss_start"
being redefined
"../usb_dev_serial.cmd", line 93: warning #10190-D: absolute symbol "bss_end"
being redefined
"../usb_dev_serial.cmd", line 92: warning #10190-D: absolute symbol "bss_start"
being redefined
"../usb_dev_serial.cmd", line 93: warning #10190-D: absolute symbol "bss_end"
being redefined
"../usb_dev_serial.cmd", line 86: warning #10261-D: section specifier matches
no sections; potential matches are consumed by section specifier at
"../usb_dev_serial.cmd", line 86
"../usb_dev_serial.cmd", line 91: warning #10423-D: No placement specified for
".bss"; a default placement will be applied.
"../usb_dev_serial.cmd", line 92: warning #10190-D: absolute symbol "bss_start"
being redefined
"../usb_dev_serial.cmd", line 93: warning #10190-D: absolute symbol "bss_end"
being redefined
"../usb_dev_serial.cmd", line 92: warning #10272-D: section relative symbols
from different output sections cannot be mixed; "bss_start" is in section
".bss", "DOT operator" is in section ".bss"
"../usb_dev_serial.cmd", line 93: warning #10272-D: section relative symbols
from different output sections cannot be mixed; "bss_end" is in section
".bss", "DOT operator" is in section ".bss"
error #10010: errors encountered during linking;
"../../../../../../../binary/armv7a/cgt_ccs/am335x/evmskAM335x/usb_dev_seria
l/usb_dev_serial.out" not built
gmake: *** [../../../../../../../binary/armv7a/cgt_ccs/am335x/evmskAM335x/usb_dev_serial/usb_dev_serial.out] Error 1
>> Compilation failure
makefile:143: recipe for target '../../../../../../../binary/armv7a/cgt_ccs/am335x/evmskAM335x/usb_dev_serial/usb_dev_serial.out' failed
gmake: Target 'all' not remade because of errors.