Part Number: AM3352
Hi all,
My customers want to do SPI boot with AM3352 custom board. This board does not have EEPROM.
Currently, the following comment is output on the console and the boot stops.
"Starting kernel ..."
Let me know the procedure for SPI boot with the above configuration.
I referred to the link below but I could not SPI boot.
http://processors.wiki.ti.com/index.php/Kernel_-_Common_Problems_Booting_Linux
https://e2e.ti.com/support/arm/sitara_arm/f/791/p/416078/1478930
https://e2e.ti.com/support/arm/sitara_arm/f/791/p/425695/1519580
They are using "am335x-evm-linux-sdk-src-04.02.00.09.tar.xz".
-------------------------console----------------------------
=> bootz $loadaddr - $fdtaddr
## Current stack ends at 0x8df25be8 * kernel: cmdline image address = 0x82000000
## Skipping init Ramdisk
## No init Ramdisk
ramdisk start = 0x00000000, ramdisk end = 0x00000000
* fdt: cmdline image address = 0x88000000
## Checking for 'FDT'/'FDT Image' at 88000000
Wrong FIT format: no description
* fdt: raw FDT blob
## Flattened Device Tree blob at 88000000
Booting using the fdt blob at 0x88000000
of_flat_tree at 0x88000000 size 0x00009365
Initial value for argc=3
Final value for argc=3
## FIT configuration was not specified
using: FDT
## initrd_high = 0x90000000, copy_to_ram = 1
ramdisk load start = 0x00000000, ramdisk load end = 0x00000000
## device tree at 88000000 ... 88009364 (len=50021 [0xC365])
Loading Device Tree to 8df18000, end 8df24364 ... OK
Initial value for argc=3
Final value for argc=3
Updating property '/ocp/ethernet@4a100000/slave@4a100200/mac-address' = 60 64 05 08 d9 ce
Updating property '/ocp/ethernet@4a100000/slave@4a100200/local-mac-address' = 60 64 05 08 d9 ce
Updating property '/ocp/ethernet@4a100000/slave@4a100300/mac-address' = 60 64 05 08 d9 d0
Updating property '/ocp/ethernet@4a100000/slave@4a100300/local-mac-address' = 60 64 05 08 d9 d0
Using machid 0x3589 from environment
## Transferring control to Linux (at address 82000000)...
Starting kernel ...
-------------------------------------------------------------------------------------
Best regards,
Sasaki