Part Number: AM5728
Other Parts Discussed in Thread: TPD12S015
Tool/software: Linux
I'm working with yocto (rocko) linux-ti-staging 4.9.69 on a beagle x15 rev C board.
I have been attempting to disable the device tree nodes of x15 features I do not use (and are not present in a custom AM572x board). In the am57xx-beagle-x15-common.dtsi I have attempted to disable the nodes labeled hdmi0, tpd12s015, sound0, and hdmi.
However when I do this and install boot & rootfs to the x15's EMMC (/dev/mmcblk1) I get the following error on boot:
VFS: Cannot open root device "mmcblk1p2" or unknown-block(0,0): error -6
<snip>
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(0,0)
I do not get a kernel panic when I use an SD Card (/dev/mmcblk0) with the same boot & rootfs. I also do not get a kernel panic when I enable (status = "okay";) hdmi0, tpd12s015, sound0, and hdmi.
Can anyone provide an explanation for what I'm doing wrong with the device tree that would result in this behavior?
Device tree changes below:
/* delete aliases for hdmi0, sound0, hdmi */
/* SNIP */
hdmi0: connector {
status = "disabled";
compatible = "hdmi-connector";
label = "hdmi";
type = "a";
port {
status = "disabled";
hdmi_connector_in: endpoint {
remote-endpoint = <&tpd12s015_out>;
};
};
};
tpd12s015: encoder {
status = "disabled";
compatible = "ti,tpd12s015";
ports {
#address-cells = <1>;
#size-cells = <0>;
port@0 {
reg = <0>;
tpd12s015_in: endpoint {
remote-endpoint = <&hdmi_out>;
};
};
port@1 {
reg = <1>;
tpd12s015_out: endpoint {
remote-endpoint = <&hdmi_connector_in>;
};
};
};
};
sound0: sound0 {
status = "disabled";
compatible = "simple-audio-card";
simple-audio-card,name = "BeagleBoard-X15";
simple-audio-card,widgets =
"Line", "Line Out",
"Line", "Line In";
simple-audio-card,routing =
"Line Out", "LLOUT",
"Line Out", "RLOUT",
"MIC2L", "Line In",
"MIC2R", "Line In";
simple-audio-card,format = "dsp_b";
simple-audio-card,bitclock-master = <&sound0_master>;
simple-audio-card,frame-master = <&sound0_master>;
simple-audio-card,bitclock-inversion;
simple-audio-card,cpu {
sound-dai = <&mcasp3>;
};
sound0_master: simple-audio-card,codec {
sound-dai = <&tlv320aic3104>;
clocks = <&clkout2_clk>;
};
};
/* SNIP */
&hdmi {
status = "disabled";
vdda-supply = <&ldo4_reg>;
port {
hdmi_out: endpoint {
remote-endpoint = <&tpd12s015_in>;
};
};
};