Part Number: AM5716
Other Parts Discussed in Thread: OMAP-L138,
Hello,
In my application, I need to use EDMA to transfer data from McASP 1 and 2. I will use channels 0, and 1 of EDMA to receive /send data from/.to McASP1. channels 2 and 3 from/to McASP2. I will need INT4 is trigered when channel0 receiving completed, and INT5 is trigered when channel 2 receiving completed. I plan to set bit 0 of shadow region register 0 for channel 0(TCC#0) and set bit 2 of shadow region register 1 for channel 2(TCC#2), so I can have two separated data transfer completion interrupt. But I could not find the event ID for shadow region channel transfer completion in AM5716 document. I remember, in omap-l138, the event id for EDMA channel transfer completion is 8.
is there a system event mapping table available just like omap-l138? or I need to do something else for mapping?
Thanks in advance!
Ron