Other Parts Discussed in Thread: SYSBIOS
Tool/software: TI-RTOS
Hello,
On the latest PDK package (version 01.08.01.06 that comes with SDK 3.02) there seems to be some duplicates that i am not sure i understand:
under the drv->stw_lld there are folders for "boards" , "devices" , "platform" ,... and the similar folder names also exist under the drv->vps->src folder
can you please explain the duplicate, what are the differences, when each of these are/should be used and under which libraries.
why would the boards and platform be under vps at all?
i will appreciate any information you can provide on explaining the above and the PDK structure in general,the split and meaning between csl, stw_lld, bsp,... (do bsp only relavnt when using sysBios while csl/stw is more generic? what about vps?)
(i tried looking at the documents published by TI but they did not provide enough information/description to answer my questions).
Thanks