Hi,
I need a setup with 3-4 stereo codecs (will probably stick with the TLV320AIC3204) for code development. Is there a way that I can connect more codes without making a pcb? Getting a TLV320AIC3204EVM for this be the way to go? I'm currently using the C5505 eZDSP USB Stick. But I'm planning to get the TMS320VC5505 Evaluation
Module (EVM) instead so that in can use C5505 USB port for USB Audio, which I can't on the stick?
Thanks,
Stefan Gram