Part Number: TMDSLCDK138
Other Parts Discussed in Thread: OMAPL138
Greetings
This is to inform that we are doing our project under DRDO on OMAP L138 LCDK Development board.
We were successfully able to run face detect demo and see output on monitor but there is one issue that I have mentioned below.
We are using emulator Standalone XDS110 and CCS7.
But the main problem is that after loading and resuming the .out file the output on monitor is coming after around 45 minutes.
Why it's coming so late??
And I have second question:
Since our project is mainly to capture image through composite input and store it, so we need to modify the code to meet our requirement.
In code there are various addresses and registers. Could anyone please guide that how to start coding for OMAPL138 or atleast a particular datasheet where we can find the registers and addresses used in code.
How to get start if I want to start at least a basic code with OMAPL138?
Kindly suggest as soon as possible
Thanks much