Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3358: UART transmission complete interrupt

Genius 5820 points

Part Number: AM3358

Hi,

I want to connect my UART to a communication partner which does not support duplex. Means sending to this device has to be signaled by a separate output. Only when this output is LOW, the other side is allowed to send an answer, when the output is HIGH the other end receives data.

My idea was to use a GPIO for this and to set it to HIGH on begin of a transmission and to set it to LOW on end of transmission. Now my question: is there an interrupt which signals "UART FIFO empty" / "transmission completed" or something like this? Only one I found was the "FIFO threshold" interrupt which does not mean transmission was completed.

Or is there a different solution to implement such a signal line which is HIGH only as long as data transfer is in progress?

Thanks!