Part Number: AM4372
Other Parts Discussed in Thread: TPS65218
Hi champs,
It does not connect to JTAG and AM4372 devices,
So it checked Power up sequence.
Error code is
Error connecting to the target:
(Error -1170 @ 0x0)
Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK).
(Emulation package 7.0.48.0)
・on the CCS
CS_DAP_DebugSS: Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 7.0.48.0)
TPS65218 RTC_PWRONRSTn VDDSHVx.pptx
(1) For the attached "TPS65218 RTC_PWRONRSTn VDDSHVx.pptx"
P1 : VDDS_RTC and RTC_PWRONRST simultaneously rise.
P2 : the waveform slightly rises at the rising edge of VDDSHVx
It is acceptable? Please let me know.
It does not use RTC now.
(2) If you have other concerns, would you please tell me?
Regards,
Shinji Ueda