- If I run a ram test and access ram directly, everything seems to run ok. I write 5’s, verify, write A’s, verify, write sequential values, and verify. I don’t get any errors doing this.
 - If I try to load an app that utilizes external memory in the linker command file, I get an error while the app is being loaded by the XDS510PLUS. The error is as follows: Cortex_A8_0: File Loader: Data verification failed at address 0x82000000 Please verify target memory and memory map.
 - If I try to load the OS from an SD card, it loads the
     TI XLoader app from the card then tries to load U-Boot, but it
     stops.  It’s like it can’t load U-Boot into RAM.
Texas Instruments X-Loader 1.44 (Dec 8 2009 - 22:58:46)
Starting OS Bootloader...