This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6748: SPI FLASH BOOT from c6748 board

Part Number: TMS320C6748
Other Parts Discussed in Thread: OMAP-L138

Hello,

I am working in tms320c6748 board. I want to use SPI flash boot. I connected S25FL064L spi flash to SPI0 pins in c6748 processor board. I checked with sfh utility to erase the chip. The sfh hangs at erasing chip

I tried with the CCS utility provided C:\ti_ccs\OMAP-L138_FlashAndBootUtils_2_40\OMAP-L138_FlashAndBootUtils_2_40\OMAP-L138\CCS\SPIWriter that goes to unknown state after reading file and info: file read complete.

Is this SPI flash compatible with the c6748? Suggest solution.

Thanks in advance.

With Regards

Shalini