This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I think that you are looking for the IIR UART register which records the interrupt event. See section 2.9 of the UART User Guide for more information.Yongquan Chen said:1,How can i judge what kind of the interrupt when an UART INT occur?receive interrupt or transmit interrupt? More detail, when i running my UART ISR program, i find that it will occur interrupt and enter UART ISR whether sending data or receiving data. In my UART ISR, how can i jude the interrupt source?
See the FCR register in the User Guide.Yongquan Chen said:2,How to configure the interrupt FIFO for DM6437? In my UART ISR, i set a counter for monitoring, i find that the program enter UART ISR when it receive 4 Bytes. Why 4 Bytes ? Could i configure it through some register? such as 16 Bytes one interrupt?