Part Number: AM4378
I'm working with a customer to integrate aspects of the Start Kit into a design. Customer has a few questions regarding potential changes to DDR3 routing.
Can you help with the following questions:
1) The Starter Kit uses blind vias in a number of places. In many cases, it is clear from the congestion a through via would have impacted routing channels needed on other layers. In other instances, a blind via was used where a through via could have been used. Based on the size and layers of the board, we can save 20-30% on our PCBs if blind or backdrilled vias are not necessary. Once we remove nets not needed by our design, we now have a much larger number of vias that could be converted to through style.
a) Were blind vias just used for signal integrity and can we convert these to through vias?
b) If for signal integrity, can we move the DDR3 routing from layer 3 to layer 6 so that the resulting via stub is very small?
2) The Starter Kit uses 4 mil traces in several areas for the DDR3 routing. Shifting these to 5 mil would give us more production flexibility. We understand the need to ensure impedance and clearance spacing requirements are met. Can we shift to 5 mil?
3) The Starter Kit uses 0 Ohm series resistors on address, clock, and a number of control strobes. We'd like to eliminate these and any associated vias added to bring the signal to the top. This seems to be very favorable because it only improves the routing, but we'd like to know if there was any purpose to these parts being added. They seem contrary to the supplied guidelines.
4) The Starter Kit uses Micron DDR3L. These parts are currently on allocation so it is possible they will not be available when we are ready to build. We are looking at second sourcing parts from ISSI as in every aspect I can see the specifications are the same. During the development phase we will migrate to lower density parts as we feel only 512MB is needed for our system.
Memory Part Numbers:
Micron Original Starter Kit part: DDR3L MT41K256M16HA-125 (-1600, 256Mx16)
Micron Prototype DDR3L MT41K256M16TW-093:P (-2133, 256Mx16)
ISSI Prototype DDR3L IS43TR16256AL-15HBL (-1333, 256Mx16)
Micron Production DDR3L MT41K128M16JT-125:K (-1600, 128Mx16)