Hi team,
I am trying to use the PinMux Tool for the AM437x. The only peripheral I have added so far is the ECAT_PRUSS1 and within that I want to enable 4 of the edio_data_in[x] lines and 4 of the edio_data_out[x]. The moment I select at least 1 of each of the input and output, I am getting an error but looking at the pin allocations, I see no reason why I should have an error.
For example, first selecting edio_data_in0 and then edio_data_out0, I am getting a "Pin conflict" which says "T21 is not valid for ECAT_PRUSS1_IOSet_1" even though I haven't yet allocated T21 for anything else yet.
Any idea what is going on here?
Here is my PinMux file for reference:/cfs-file/__key/communityserver-discussions-components-files/791/AM437x.pinmux
Regards,
Akash Patel