Part Number: BEAGLEBOARD-X15
Other Parts Discussed in Thread: BEAGLEBOARD-X15, AM5728
Hi
environment:
hardware: TI AM5728 BeagleBoard-X15 board
software: android O (SDK is ti-processor-sdk-android-am57xx-evm-04.02.00.09-Linux-x86-Install.bin)
issue:
In ADB mode, I try to execute "adb reboot bootloader" , but the board can not enter fastboot mode. the board still boot android system.
there are some doubtful kernel log. the log as below
[ 21.579611] nf_conntrack: automatic helper assignment is deprecated and it will be removed soon. Use the iptables CT target to attach helpers instead.
[ 44.058069] init: reboot-bootloader: Error writing bootloader_message: failed to find /misc partition
[ 44.067439] init: Reboot start, reason: reboot,bootloader, rebootTarget: bootloader
[ 44.075677] init: Shutdown timeout: 6
Thanks and Regards.
qu shenghui