This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: TPS65910 connections

Guru 10305 points

Part Number: AM3352

Hi Sitara support Team,

 

I would like to make sure the connection of AM335x to TPS65910AA1
in TPS65910Ax User's Guide for AM335x Processors.

http://www.ti.com/lit/ug/swcu093f/swcu093f.pdf

"INT1" and "SLEEP" pin of TPS65910AA1 connect to "GPIO0_8" and
"GPIO0_9" of AM335x in the following figure 1.

If  "GPIO0_8" and "GPIO0_9" of AM335x are used as other usages,
what is the guideline/standard to select the alternative pins
connecting "INT1" and "SLEEP" pin of TPS65910AA1?  

Can they select any free pins if their pin Attributes in AM335x Datasheet are same?

Best regards,
Kanae