This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: Can't skip empty NAND to boot from MMC

Part Number: AM3352

stomer use new NAND device 29F8G08ABABA, set boot mode to 10011b, NAND is empty,  insert TF card with boot image, power up, the board can't boot up.

but with old NAND devcie S34ML08G201TF100, same configuration with empty NAND, it can boot from TF card. 

Change boot mode to 10111b, board can boot from TF card with empty 29F8G08ABABA. then burn NAND, and change boot mode back to 10011b to boot from NAND, the board can boot from NAND 29F8G08ABABA. so the 29F8G08ABABA can work as AM3352 boot device.

Why ROM can't skip empty NAND 29F8G08ABABA?