Other Parts Discussed in Thread: CCSTUDIO
Hai
I am facing lot of problems in my DM6437-EVM board
Problem-1:Flash program is not running (When i power up the board i connect the input and output but it does not do anything as told in the document)
steps taken
using flash burn utility i burn the flash program fron the installed folder
C:\dvsdk_1_01_00_15\flashburn_files
and keep all boot mode switchs as mentioned in the document....
But i have got nothing........
Problem-2: I try to run the program given the in examples
D:\dvsdk_1_01_00_15\examples
some 6 programs are there but it is was also not running
steps taken
i have changed the memory using the jumper settings JP2
i tried in all the memories like flash,SRAM,NAND but it loads the program , if run nothing was happening
all the programs are loading properly, when i run it does int give anything, to test i have added a printf it is also not working.....
The only thing i am getting output is
From the installed folder
C:\CCStudio_v3.3\boards\evmdm6437_v2\tests\
all the test program was running and proper output was comming , This only ensure me that my board is working properly.....
So kindly give me a solution for the above mentioned 2 problems
regards