This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/EVMK2G: QSPI Writer

Part Number: EVMK2G

Tool/software: Code Composer Studio

I have problems to write the MLO and APP to the QSPI flash of my K2G EVM Board.

I used this page: 

Is this solution working ?

  • The team is notified. They will post their feedback directly here.

    BR
    Tsvetolin Shulev
  • Richars,

    You are refering to the correct document for flashing QSPI. Can please provide more details about the issue that you are running into

    • Can you please indicate what version of the SDK you are using. there was a issue with QSPI Writer in PRSDK 4.0 where the Write command was not erasing the blocks before writing. It was fixed in all subsequent releases
    • Did you Fat format the SD Card and copy config file. and rename the MLO file to boot as recommended in the SDK.
    • When you run the flash writer, do you see any UART messages on the UART to indicate where it failed.
    • How do you know that the images were not programmed. Did you chnage the boot switches to QSPI boot and check or did the flash writer indicate an error.

    Regards,

    Rahul

  • Thank you for replay. Sorry I have found the error. You have to choose No Boot option while flashing.

    Best regards

    Richard


    ---Closed---