Other Parts Discussed in Thread: OMAP-L138
Dear Forum, We are in the process of going as low power as possible while in deepsleep on our current custom design based on the OMAP-L138. The first series of board is using a device revision 'A' (silicon revision 1.1). We run Linux on the system which is based on the latest PSP. My first question is : What are the expected power consumption gains between a rev A and B, if any ? So far we didn't reach the expected target consumption and we are working hard to go as low as possible. Current global power-consumption values in deepsleep are : 29mA @ 5V = 145mW. We'd like to reduce down to at least a third of that. To be able to compare our results with what others have reached I would be interested to know someone has the figures for the OMAP-L138 EVM and what power consumption we can measure on that board (the LogicPD one) while in DEEPSLEEP. (When using the SOM idependently). I'm more interested on the global power consumption of the board on the main power rail that just the OMAP core consumption. But any information would be useful. I would also be interested to know if there are any components (peripherals) appart from the USB 2.0 PHY and SATA PHY that should be switched off explicitly before going to deepsleep to reduce the power consumption further down. E.g. Will the power consumption be different if I disable the DSP before going to deepsleep (using the PSC features) or going to deepsleep switches off the DSP anyway. Our design doesn't use the internal RTC but has an external one so we can leverage the DEEPSLEEP feature to wake-up from deep sleep using an external event (a button is pressed) or an rtc alarm (system must wake up every week to check it's still alive). Are there any special action that must be taken to switch off the internal RTC ? Also we don't use the TPS65070 that is on the EVM but the TPS65023 PMIC. Any help / tips to get the power down will be much appreciated. Best regards, Christophe