This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRA756: Display Subsystem

Part Number: DRA756

Hi,

I have a query regarding display ports for Jacinto6 Plus. 

According to TRM, there are 3 LCD outputs, providing support for MIPI DPI 2.0, or BT-656 or BT-1120.

Do these display ports support LVDS interface?

Can you give me a list of the interfaces supported by the display ports?

Thanks,

Mandar

  • Mandar,

    Display does not support LVDS interface directly, you need to connect external serializer to convert to LVDS output.

    Essentially J6+ supports HDMI and 3 DPI outputs. DPI outputs can be used to get MIPI DPI 2.0 or BT656/BT1120 output format.

    Regards,
    Brijesh