This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Memory problem



Hi,

I am using a custom board with dm355 and I have some questions about RAM memory.

Booting my board from NFS and using the "free" command I get:

# free
                    total         used         free       shared      buffers
  Mem:        77940        34864        43076            0           20
  Swap:            0            0            0
  Total:        77940        34864        43076

But booting from NAND flash(uImage and ramdisk), I get:

  # free
                    total         used         free       shared      buffers
  Mem:        77940        64008        13932            0        31764
  Swap:            0            0            0
  Total:        77940        64008        13932

 

Can anyone please tell why there are 30MB of difference between them? My ramdisk.gz is 11MB.

Can I do anything to free that memory? I really need that memory free.

Hope anyone can help me.

Thanks!