This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TDA2P-ACD: BUILD_MACHINE flag for Linux build

Part Number: TDA2P-ACD

Tool/software: Linux

Hello All,

I am currently working with TDA2P EVM and Processor SDK 3.2 with Linux on A15. I have built PDK 3.2 for "tda2px_evm_linux_all" configuration.

My machine is a 64-bit machine and I have build PDK with BUILD_MACHINE=64BIT. But in Rules.make, for "BUILD_MACHINE" flag, it is mentioned that "Set BUILD_MACHINE to 32BIT as required, this is needed only if A15_TARGET_OS is going to be Linux".

I am a bit confused here whether to keep BUILD_MACHINE as 64BIT or 32BIT for A15_TARGET_OS as my machine is 64-bit.

Regards,

Abhay