Part Number: AM3358
Tool/software: Linux
Hello
I have designed a custom board of AM3358 based on AM335X General Purpose EVM in which I have configured the SPI0 as slave (changing the register values in the kernel).
The problem is when a master is driving the chip select signal and sck signal , AM3358's SPI port is pulling the lines low and making the Chip select and sck signals run from 1V to 0V instead of 3.3V to 0V.
How to avoid this to happen?
Regards
Mad_hu