Part Number: PROCESSOR-SDK-AM335X
Other Parts Discussed in Thread: TLK110, TPS65910
Good morning,
we would like to develop a SPI-EtherNet/IP interface.
Our need for operating temperature is -40 85°C.
-So, we think that probably our solution could be a Sitara AM335x product, but can You please assist us in the choice of the most suitable AM335x for us?
It is important for us also to have all the avalable documentation about Ethernet/IP, both for correct hadrware design and also Ethernet/ip code example.
- Then we would like also to procure the evaluation board in order to perform the first tests: is there a suitable evaluation board?
- Will it be also possible to realize a SPI-EtherCAT interface?
- Is it also needed TLK110 and TPS65910?
Thank You,
kind regards