Part Number: TMS320DM8168
Hi,
We are planing to use DM8168 in our project. We need HD Video(upto 1080p30) processing. But due to pin constraints, only 8bit input mode(with interleaved Y/C data input) can be used.
But according to TRM, following 8 bit input modes are only supported:
8-bit input ports:
– A single non-multiplexed CIF/480i/480p/720p/1080i Y/C data
– Up to 2-stream multiplexed ED (480p) Y/C data
– Up to 4-stream multiplexed SD (480i) Y/C data
– Up to 16-stream multiplexed CIF Y/C data
According to above statements, only 1080i is supported in single non multiplexed 8 bit input port. Is it not possible to capture 1080p24,25,30 formats using 8 bit input mode ?
Regards,
Pranay kumar