Other Parts Discussed in Thread: OMAP-L138
Hi,
We are using LogicPD Omap-l138 Eval. board and I was trying to load the NOR Flash with the UBL + Uboot. I found two dir. with the utilities to do that. One in PSP
/DaVinci-PSP-SDK-03.20.00.12/\src\boot-strap\armubl-03.20.00.12 and the other one in \OMAP-L138_FlashAndBootUtils_2_29\OMAP-L138 which has both the host side and also the target side. It seems that we need both the host and target together. If I wanted to change the FLash memory map to make the serial loader to work with our on-board NOR Flash which has different size and address, what files do I need to modify? I think I need to modify files such as \OMAP-L138_FlashAndBootUtils_2_29\OMAP-L138\CCS\UBL_ARM\UBL.cmd and \OMAP-L138_FlashAndBootUtils_2_29\OMAP-L138\device.mak, \OMAP-L138_FlashAndBootUtils_2_29\OMAP-L138\GNU\ublARM_ubl.cmd & ARM_ubl.lds
Also, when I compared the file \DaVinci-PSP-SDK-03.20.00.12\src\kernel\linux-03.20.00.12\arch\arm\mach-davinci\board-da850-evm.c SPI flash partitions
static struct mtd_partition spi_flash_partitions[] = {
[0] = {
.name = "U-Boot",
.offset = 0,
.size = SZ_256K,
.mask_flags = MTD_WRITEABLE,
},
[1] = {
.name = "U-Boot Environment",
.offset = MTDPART_OFS_APPEND,
.size = SZ_64K,
.mask_flags = MTD_WRITEABLE,
},
[2] = {
.name = "Linux",
.offset = MTDPART_OFS_NXTBLK,
.size = SZ_8M - (SZ_256K + SZ_64K + SZ_64K),
.mask_flags = 0,
},
[3] = {
.name = "MAC Address",
.offset = MTDPART_OFS_NXTBLK,
.size = SZ_64K,
.mask_flags = MTD_WRITEABLE,
.setup = davinci_get_mac_addr,
.context = (void *)0,
},
};
it didn't match the one from LogicPD U-boot lab memory map:
0x000000 ARM AIS Bootloader (arm-api-ais.bin)
0x010000 U-Boot prepended with config (u-boot.bin)
0xc08000 Linux Image (uImage)
0x28000 File system (ramdisk-base.gz)
I can see the kernel when it runs it creates the spi_flash_partitions, now do I need to change the uboot bootargs to write to these partions or to above memory map?
Does the partions in board-da850-evm.c file need to match the address and the size of Flash that I use to write the UBL and the u-boot through Serial Flash loader?
Thanks for any help,
Alex