Tool/software: Linux
Hello all
We use DS921 for 24bit RGB on J6 and DS948 for lvds display,
We currently need one channel for pwm input , and seems only i2s channle is avaliable ,
so we use GPO7_I2S_WC in DS921 and GPO7_I2S_WC in DS948
Our 24K pwm can get in DS921 GPO7 ,while the GPO7 in DS928 can not get the output
I want to know ,
If ds921 I2S channel can pair with DS948 I2S channel ? if only I2S WC signal is avaible , does this works ?
If this solution can work , how to set the i2c register ?
If this solution can not work , does any other way to get a 24k signal output to DS948 ?
We notice the DS948 can support 4 channel i2s ,does this two chip have the same time slot id for i2s WC channle ?
Thanks and regards