Hi everybody,
I have just installed the TI_EVM_3530 BSP, it runs, it is visible on VS2005, I can open the prebuilt solution, I also can create a new project with this BSP.
Still, I have 2 problems:
The first one is that in the catalog items view, in the tree third party, I have BSP and PowerVR. From BSP, I can see my BSP "TI_EVM_3530" that is checked, but from it, nothing is going out (i.e it is the end of the tree, instead of opening on the device drivers...).
the second problem, is when I decided to build my OS anyway, despite the first issue. and then, I get the fatal error as shown in the title of this post: "BUILD: [01:0000000187:ERRORE] C:\WINCE600\platform\TI_EVM_3530\src\inc\bsp.h(26) : fatal error C1083: Cannot open include file: 'oal.h': No such file or directory"
The OAL.h seems to miss, and I can't understand why since I have installed the BSP as it is.
Maybe the 2 issues are linked together, I really dont know, if anyone is able to help me, it would be welcome....!! :-)))))
thank you
Nathaniel