Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/AM3358: U-boot not detecting NAND

Part Number: AM3358

Tool/software: Linux

Hi,

SDK used is 4.02.00.09 We have custom board based on the AM3358 with design somewhat similar to beaglebone. The design also includes Micron NAND flash and a device tree descriptor contains pin mux definitions and timings to reflect our design. When we load Linux, the NAND is properly recognized and partitions can be mounted and accessed. However, When we use the same device tree descriptor for use with U-boot and based on original am335xevm_defconfig configurations, the NAND is not recognized. The chip ID values don't seem to be read correctly. Suspicion is that the issue is in timers configuration. For U-boot, he clock configuration is the same as on the EVM, the 24MHz clock provides input to timer2 that is supposedly used for measuring the timing delays but the timings calculated don't seem to match what is defined in device tree even close. The PLL dividers and other settings seem to be hardcoded in the BSP sources. What do we need to do for the U-boot to properly use the device tree configuration for the NAND?

Thank you,

Roman

  • Hello Roman,

    Did you put the NAND device node descriptor in <Processor SDK>/board-support/u-boot-<version>/arch/arm/dts/am335x-boneblack.dts?
    Have you aligned your NAND's pinmux and configuration parameters in <Processor SDK>/board-support/u-boot-<version>/board/ti/am335x/mux.c and <Processor SDK>/board-support/u-boot-<version>/include/configs/am335x_evm.h? The detection problem can be caused by the parameters on these files.

    Best regards,
    Kemal

  • Hi Kemal,

    I have created my own dts file and specified in u-boot config that this is the only file in the list. So as far as I am concerned, it is picked up and used. The mux.c file in u-boot/board/ti/am335x directory is not even compiled as part of the build. This is I believe due to the fact that use of device tree descriptors was specified in u-boot config as oppose to using hardcoded stuff. Doing anything with the mux.c file has absolutely no effect since it is not compiled/linked in.

    Thanks,

    Roman

  • So, what if the object file is generated to a different directory, rather than the current one, like the SPL does in U-Boot?

    <Processor SDK>/board-support/u-boot-<version>/spl/board/ti/am335x/mux.o gets generated from <Processor SDK>/board-support/u-boot-<version>/board/ti/am335x/mux.c and the recent changes on <Processor SDK>/board-support/u-boot-<version>/board/ti/am335x/mux.c won't be reflected on incremental builds, if you are not cleaning it.

  • The object file is not generated. As I said before, the file is not even compiled. And I can see why. The Makefile in board/ti/am335x states:

    ifeq ($(CONFIG_SKIP_LOWLEVEL_INIT),)
    obj-y := mux.o
    endif

    obj-y += board.o

    So the mux.o is only included with CONFIG_SKIP_LOWLEVEL_INIT undefined.
    Tracing it back, I find in include/configs/ti_am335x_common.h in lines 65-80:
    .....
    /*
    * Since SPL did pll and ddr initialization for us,
    * we don't need to do it twice.
    */
    #if !defined(CONFIG_SPL_BUILD) && !defined(CONFIG_NOR_BOOT)
    #define CONFIG_SKIP_LOWLEVEL_INIT
    #endif

    /*
    * When building U-Boot such that there is no previous loader
    * we need to call board_early_init_f. This is taken care of in
    * s_init when we have SPL used.
    */
    #if !defined(CONFIG_SKIP_LOWLEVEL_INIT) && !defined(CONFIG_SPL)
    #define CONFIG_BOARD_EARLY_INIT_F
    #endif
    ....

    That obviously means that I have to have SPL build or NOR boot enabled if the CONFIG_SKIP_LOWLEVEL_INIT is to be undefined. Neither of these are the case in our project. The SPL is completely disabled since we have our own first stage bootloader that is used to load u-boot. And the NOR boot is only optional.

    But that's still somewhat beside the point. The u-boot should use the pinmux as defined in the device tree description. Not the hardcoded mux.c file.

    Thanks,
    Roman
  • Hi Roman,
    SPL does the pin-muxing. u-boot does not. If you look in System.map, you will not find the pin-muxing routines.

    Steve K.
  • Hi Steve,

    We are not using SPL at all but do have proprietary first stage bootloader. I'll add the muxing there and try it.

    Will keep you posted.

    Thanx,

    Roman

  • Si I have added the pin muxing in our first stage bootloader that loads and starts u-boot as follows:

    unsigned int NANDPinMuxSetup(void)
    {
    /* GPMC_AD0 */
    HWREG(SOC_CONTROL_REGS + CONTROL_CONF_GPMC_AD(0)) =
    ( 0 << CONTROL_CONF_GPMC_AD0_CONF_GPMC_AD0_MMODE_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_AD0_CONF_GPMC_AD0_PUDEN_SHIFT) |
    ( 0 << CONTROL_CONF_GPMC_AD0_CONF_GPMC_AD0_PUTYPESEL_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_AD0_CONF_GPMC_AD0_RXACTIVE_SHIFT);

    /* GPMC_AD1 */
    HWREG(SOC_CONTROL_REGS + CONTROL_CONF_GPMC_AD(1)) =
    ( 0 << CONTROL_CONF_GPMC_AD1_CONF_GPMC_AD1_MMODE_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_AD1_CONF_GPMC_AD1_PUDEN_SHIFT)|
    ( 0 << CONTROL_CONF_GPMC_AD1_CONF_GPMC_AD1_PUTYPESEL_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_AD1_CONF_GPMC_AD1_RXACTIVE_SHIFT) ;
    /* GPMC_AD2 */
    HWREG(SOC_CONTROL_REGS + CONTROL_CONF_GPMC_AD(2)) =
    ( 0 << CONTROL_CONF_GPMC_AD2_CONF_GPMC_AD2_MMODE_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_AD2_CONF_GPMC_AD2_PUDEN_SHIFT)|
    ( 0 << CONTROL_CONF_GPMC_AD2_CONF_GPMC_AD2_PUTYPESEL_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_AD2_CONF_GPMC_AD2_RXACTIVE_SHIFT) ;
    /* GPMC_AD3 */
    HWREG(SOC_CONTROL_REGS + CONTROL_CONF_GPMC_AD(3)) =
    ( 0 << CONTROL_CONF_GPMC_AD3_CONF_GPMC_AD3_MMODE_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_AD3_CONF_GPMC_AD3_PUDEN_SHIFT)|
    ( 0 << CONTROL_CONF_GPMC_AD3_CONF_GPMC_AD3_PUTYPESEL_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_AD3_CONF_GPMC_AD3_RXACTIVE_SHIFT) ;
    /* GPMC_AD4 */
    HWREG(SOC_CONTROL_REGS + CONTROL_CONF_GPMC_AD(4)) =
    ( 0 << CONTROL_CONF_GPMC_AD4_CONF_GPMC_AD4_MMODE_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_AD4_CONF_GPMC_AD4_PUDEN_SHIFT)|
    ( 0 << CONTROL_CONF_GPMC_AD4_CONF_GPMC_AD4_PUTYPESEL_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_AD4_CONF_GPMC_AD4_RXACTIVE_SHIFT) ;
    /* GPMC_AD5 */
    HWREG(SOC_CONTROL_REGS + CONTROL_CONF_GPMC_AD(5)) =
    ( 0 << CONTROL_CONF_GPMC_AD5_CONF_GPMC_AD5_MMODE_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_AD5_CONF_GPMC_AD5_PUDEN_SHIFT)|
    ( 0 << CONTROL_CONF_GPMC_AD5_CONF_GPMC_AD5_PUTYPESEL_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_AD5_CONF_GPMC_AD5_RXACTIVE_SHIFT) ;
    /* GPMC_AD6 */
    HWREG(SOC_CONTROL_REGS + CONTROL_CONF_GPMC_AD(6)) =
    ( 0 << CONTROL_CONF_GPMC_AD6_CONF_GPMC_AD6_MMODE_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_AD6_CONF_GPMC_AD6_PUDEN_SHIFT) |
    ( 0 << CONTROL_CONF_GPMC_AD6_CONF_GPMC_AD6_PUTYPESEL_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_AD6_CONF_GPMC_AD6_RXACTIVE_SHIFT) ;
    /* GPMC_AD7 */
    HWREG(SOC_CONTROL_REGS + CONTROL_CONF_GPMC_AD(7)) =
    ( 0 << CONTROL_CONF_GPMC_AD7_CONF_GPMC_AD7_MMODE_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_AD7_CONF_GPMC_AD7_PUDEN_SHIFT) |
    ( 0 << CONTROL_CONF_GPMC_AD7_CONF_GPMC_AD7_PUTYPESEL_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_AD7_CONF_GPMC_AD7_RXACTIVE_SHIFT) ;/* GPMC_WAIT0 */

    HWREG(SOC_CONTROL_REGS + CONTROL_CONF_GPMC_WAIT0) =
    ( 0 << CONTROL_CONF_GPMC_WAIT0_CONF_GPMC_WAIT0_MMODE_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_WAIT0_CONF_GPMC_WAIT0_PUDEN_SHIFT) |
    ( 0 << CONTROL_CONF_GPMC_WAIT0_CONF_GPMC_WAIT0_PUTYPESEL_SHIFT)|
    ( 1 << CONTROL_CONF_GPMC_WAIT0_CONF_GPMC_WAIT0_RXACTIVE_SHIFT);

    /* GPMC_WPN */
    HWREG(SOC_CONTROL_REGS + CONTROL_CONF_GPMC_WPN) =
    ( 7 << CONTROL_CONF_GPMC_WPN_CONF_GPMC_WPN_MMODE_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_WPN_CONF_GPMC_WPN_PUDEN_SHIFT) |
    ( 0 << CONTROL_CONF_GPMC_WPN_CONF_GPMC_WPN_PUTYPESEL_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_WPN_CONF_GPMC_WPN_RXACTIVE_SHIFT);

    /* GPMC_CS0 */
    HWREG(SOC_CONTROL_REGS + CONTROL_CONF_GPMC_CSN(0)) =
    ( 0 << CONTROL_CONF_GPMC_CSN0_CONF_GPMC_CSN0_MMODE_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_CSN0_CONF_GPMC_CSN0_PUDEN_SHIFT)|
    ( 0 << CONTROL_CONF_GPMC_CSN0_CONF_GPMC_CSN0_PUTYPESEL_SHIFT)|
    ( 0 << CONTROL_CONF_GPMC_CSN0_CONF_GPMC_CSN0_RXACTIVE_SHIFT);

    /* GPMC_ALE */
    HWREG(SOC_CONTROL_REGS + CONTROL_CONF_GPMC_ADVN_ALE) =
    ( 0 << CONTROL_CONF_GPMC_ADVN_ALE_CONF_GPMC_ADVN_ALE_MMODE_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_ADVN_ALE_CONF_GPMC_ADVN_ALE_PUDEN_SHIFT) |
    ( 0 << CONTROL_CONF_GPMC_ADVN_ALE_CONF_GPMC_ADVN_ALE_PUTYPESEL_SHIFT) |
    ( 0 << CONTROL_CONF_GPMC_ADVN_ALE_CONF_GPMC_ADVN_ALE_RXACTIVE_SHIFT);

    /* GPMC_BE0N_CLE */
    HWREG(SOC_CONTROL_REGS + CONTROL_CONF_GPMC_BE0N_CLE) =
    ( 0 << CONTROL_CONF_GPMC_BE0N_CLE_CONF_GPMC_BE0N_CLE_MMODE_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_BE0N_CLE_CONF_GPMC_BE0N_CLE_PUDEN_SHIFT) |
    ( 0 << CONTROL_CONF_GPMC_BE0N_CLE_CONF_GPMC_BE0N_CLE_PUTYPESEL_SHIFT) |
    ( 0 << CONTROL_CONF_GPMC_BE0N_CLE_CONF_GPMC_BE0N_CLE_RXACTIVE_SHIFT);

    /* GPMC_OEN_REN */
    HWREG(SOC_CONTROL_REGS + CONTROL_CONF_GPMC_OEN_REN) =
    ( 0 << CONTROL_CONF_GPMC_OEN_REN_CONF_GPMC_OEN_REN_MMODE_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_OEN_REN_CONF_GPMC_OEN_REN_PUDEN_SHIFT) |
    ( 0 << CONTROL_CONF_GPMC_OEN_REN_CONF_GPMC_OEN_REN_PUTYPESEL_SHIFT) |
    ( 0 << CONTROL_CONF_GPMC_OEN_REN_CONF_GPMC_OEN_REN_RXACTIVE_SHIFT);

    /* GPMC_WEN */
    HWREG(SOC_CONTROL_REGS + CONTROL_CONF_GPMC_WEN) =
    ( 0 << CONTROL_CONF_GPMC_WEN_CONF_GPMC_WEN_MMODE_SHIFT) |
    ( 1 << CONTROL_CONF_GPMC_WEN_CONF_GPMC_WEN_PUDEN_SHIFT) |
    ( 0 << CONTROL_CONF_GPMC_WEN_CONF_GPMC_WEN_PUTYPESEL_SHIFT) |
    ( 0 << CONTROL_CONF_GPMC_WEN_CONF_GPMC_WEN_RXACTIVE_SHIFT);

    return TRUE;
    }

    That I hope is the proper match for the device tree version that works fine under Linux:

    nandflash_pins_s0: nandflash_pins_s0 {
    pinctrl-single,pins = <
    AM33XX_IOPAD(0x800, PIN_INPUT | MUX_MODE0) /* gpmc_ad0.gpmc_ad0 */
    AM33XX_IOPAD(0x804, PIN_INPUT | MUX_MODE0) /* gpmc_ad1.gpmc_ad1 */
    AM33XX_IOPAD(0x808, PIN_INPUT | MUX_MODE0) /* gpmc_ad2.gpmc_ad2 */
    AM33XX_IOPAD(0x80c, PIN_INPUT | MUX_MODE0) /* gpmc_ad3.gpmc_ad3 */
    AM33XX_IOPAD(0x810, PIN_INPUT | MUX_MODE0) /* gpmc_ad4.gpmc_ad4 */
    AM33XX_IOPAD(0x814, PIN_INPUT | MUX_MODE0) /* gpmc_ad5.gpmc_ad5 */
    AM33XX_IOPAD(0x818, PIN_INPUT | MUX_MODE0) /* gpmc_ad6.gpmc_ad6 */
    AM33XX_IOPAD(0x81c, PIN_INPUT | MUX_MODE0) /* gpmc_ad7.gpmc_ad7 */

    AM33XX_IOPAD(0x870, PIN_INPUT | MUX_MODE0) /* gpmc_wait0.gpmc_wait0 */

    AM33XX_IOPAD(0x874, PIN_INPUT | MUX_MODE7) /* gpmc_wpn.gpio0_30 */
    AM33XX_IOPAD(0x87c, PIN_OUTPUT | MUX_MODE0) /* gpmc_csn0.gpmc_csn0 */
    AM33XX_IOPAD(0x890, PIN_OUTPUT | MUX_MODE0) /* gpmc_advn_ale.gpmc_advn_ale */
    AM33XX_IOPAD(0x894, PIN_OUTPUT | MUX_MODE0) /* gpmc_oen_ren.gpmc_oen_ren */
    AM33XX_IOPAD(0x898, PIN_OUTPUT | MUX_MODE0) /* gpmc_wen.gpmc_wen */
    AM33XX_IOPAD(0x89c, PIN_OUTPUT | MUX_MODE0) /* gpmc_be0n_cle.gpmc_be0n_cle */
    >;
    };

    However, even with the pin muxing set, the u-boot still stalls when trying to reset the NAND on first access to read IDs. Here is the u-boot log:

    initcall: 8080eaeb (relocated to bff52aeb)
    initcall: 8080eaeb (relocated to bff52aeb)
    initcall: 8080eaeb (relocated to bff52aeb)
    initcall: 8080eeb1 (relocated to bff52eb1)
    initcall: 8080eaeb (relocated to bff52aeb)
    initcall: 8080ef5d (relocated to bff52f5d)
    NAND: uclass_find_device_by_seq: 0 -1
    uclass_find_device_by_seq: 0 0
    gpmc@50000000 - -1 -1
    - not found
    OF: ** translation for device gpmc@50000000 **
    OF: bus is default (na=1, ns=1) on ocp
    OF: translating address: 00000050
    OF: parent bus is default (na=1, ns=1) on
    OF: no ranges, 1:1 translation
    OF: parent translation for: 00000000
    OF: with offset: 1342177280
    OF: one level translation: 00000050
    OF: reached root node
    fdtdec_get_int: gpmc,num-cs: 0x7 (7)
    fdtdec_get_int: reg: 0x0 (0)
    fdtdec_get_int: nand-bus-width: 0x8 (8)
    fdtdec_lookup_phandle: ti,elm-id
    nand: selected OMAP_ECC_BCH8_CODE_HW
    RR elm_init
    RR elm_init done
    RR OMAP_ECC_BCH8_CODE_HW done
    uclass_find_device_by_seq: 0 -1
    uclass_find_device_by_seq: 0 0
    timer@48040000 - -1 -1
    timer@48042000 - -1 -1
    timer@48044000 - -1 -1
    timer@48046000 - -1 -1
    timer@48048000 - -1 -1
    timer@4804a000 - -1 -1
    - not found
    fdtdec_get_int: clock-frequency: 0x2dc6c0 (3000000)
    OF: ** translation for device timer@48040000 **
    OF: bus is default (na=1, ns=1) on ocp
    OF: translating address: 00000448
    OF: parent bus is default (na=1, ns=1) on
    OF: no ranges, 1:1 translation
    OF: parent translation for: 00000000
    OF: with offset: 1208221696
    OF: one level translation: 00000448
    OF: reached root node

    The output above ends with timer2 being initialized and used as timer for the NAND access delays as per code in drivers/mtd/nand/nand_base.c:

    case NAND_CMD_RESET:
    if (chip->dev_ready)
    break;
    udelay(chip->chip_delay);
    chip->cmd_ctrl(mtd, NAND_CMD_STATUS, NAND_CTRL_CLE | NAND_CTRL_CHANGE);
    chip->cmd_ctrl(mtd,NAND_CMD_NONE, NAND_NCE | NAND_CTRL_CHANGE);
    /* EZ-NAND can take upto 250ms as per ONFi v4.0 */
    nand_wait_status_ready(mtd, 250);
    return;

    The access times out after 400s (if not interrupted by watchdog reset). So there are obviously several issues here even with the pin muxing set in FSB/SPL. The chip access fails and the timing doesn't seem to be setup properly albeit configuration being the same as the am335x evm board. For reverence, here is the whole device tree used in both, u-boot and linux. And I stress again, it works perfectly fine in linux and we can read/write and access the nand partitions.


    /*
    * basic OBC DTS
    */

    /dts-v1/;

    #include "am33xx.dtsi"
    #include <dt-bindings/interrupt-controller/irq.h>
    /* #include "am335x-bone-common.dtsi" */

    / {
    model = "TI AM335x CSYS";
    compatible = "ti,am335x-obc", "ti,am33xx";

    memory@80000000 {
    device_type = "memory";
    reg = <0x80000000 0x40000000>; /* 256 MB */
    };

    chosen {
    stdout-path = &uart0;
    };

    };

    &rtc {
    status = "disabled";
    ti,hwmods = "disabled";
    };

    &am33xx_pinmux {
    pinctrl-names = "default";
    pinctrl-0 = <&clkout2_pin>;

    i2c0_pins: pinmux_i2c0_pins {
    pinctrl-single,pins = <
    0x188 (PIN_INPUT_PULLUP | MUX_MODE0) /* i2c0_sda.i2c0_sda */
    0x18c (PIN_INPUT_PULLUP | MUX_MODE0) /* i2c0_scl.i2c0_scl */
    >;
    };

    i2c1_pins: pinmux_i2c1_pins {
    pinctrl-single,pins = <
    0x158 (PIN_INPUT_PULLUP | MUX_MODE2) /* spi0_d1.i2c1_sda */
    0x15c (PIN_INPUT_PULLUP | MUX_MODE2) /* spi0_cs0.i2c1_scl */
    >;
    };

    uart0_pins: pinmux_uart0_pins {
    pinctrl-single,pins = <
    AM33XX_IOPAD(0x970, PIN_INPUT_PULLUP | MUX_MODE0) /* uart0_rxd.uart0_rxd */
    AM33XX_IOPAD(0x974, PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* uart0_txd.uart0_txd */
    >;
    };

    uart1_pins: pinmux_uart1_pins {
    pinctrl-single,pins = <
    AM33XX_IOPAD(0x978, PIN_INPUT | MUX_MODE0) /* uart1_ctsn.uart1_ctsn */
    AM33XX_IOPAD(0x97C, PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* uart1_rtsn.uart1_rtsn */
    AM33XX_IOPAD(0x980, PIN_INPUT_PULLUP | MUX_MODE0) /* uart1_rxd.uart1_rxd */
    AM33XX_IOPAD(0x984, PIN_OUTPUT_PULLDOWN | MUX_MODE0) /* uart1_txd.uart1_txd */
    >;
    };

    clkout2_pin: pinmux_clkout2_pin {
    pinctrl-single,pins = <
    AM33XX_IOPAD(0x9b4, PIN_OUTPUT_PULLDOWN | MUX_MODE3) /* xdma_event_intr1.clkout2 */
    >;
    };

    nandflash_pins_s0: nandflash_pins_s0 {
    pinctrl-single,pins = <
    AM33XX_IOPAD(0x800, PIN_INPUT | MUX_MODE0) /* gpmc_ad0.gpmc_ad0 */
    AM33XX_IOPAD(0x804, PIN_INPUT | MUX_MODE0) /* gpmc_ad1.gpmc_ad1 */
    AM33XX_IOPAD(0x808, PIN_INPUT | MUX_MODE0) /* gpmc_ad2.gpmc_ad2 */
    AM33XX_IOPAD(0x80c, PIN_INPUT | MUX_MODE0) /* gpmc_ad3.gpmc_ad3 */
    AM33XX_IOPAD(0x810, PIN_INPUT | MUX_MODE0) /* gpmc_ad4.gpmc_ad4 */
    AM33XX_IOPAD(0x814, PIN_INPUT | MUX_MODE0) /* gpmc_ad5.gpmc_ad5 */
    AM33XX_IOPAD(0x818, PIN_INPUT | MUX_MODE0) /* gpmc_ad6.gpmc_ad6 */
    AM33XX_IOPAD(0x81c, PIN_INPUT | MUX_MODE0) /* gpmc_ad7.gpmc_ad7 */

    AM33XX_IOPAD(0x870, PIN_INPUT | MUX_MODE0) /* gpmc_wait0.gpmc_wait0 */

    AM33XX_IOPAD(0x874, PIN_INPUT | MUX_MODE7) /* gpmc_wpn.gpio0_30 */
    AM33XX_IOPAD(0x87c, PIN_OUTPUT | MUX_MODE0) /* gpmc_csn0.gpmc_csn0 */
    AM33XX_IOPAD(0x890, PIN_OUTPUT | MUX_MODE0) /* gpmc_advn_ale.gpmc_advn_ale */
    AM33XX_IOPAD(0x894, PIN_OUTPUT | MUX_MODE0) /* gpmc_oen_ren.gpmc_oen_ren */
    AM33XX_IOPAD(0x898, PIN_OUTPUT | MUX_MODE0) /* gpmc_wen.gpmc_wen */
    AM33XX_IOPAD(0x89c, PIN_OUTPUT | MUX_MODE0) /* gpmc_be0n_cle.gpmc_be0n_cle */
    >;
    };

    };

    &uart0 {
    pinctrl-names = "default";
    pinctrl-0 = <&uart0_pins>;

    status = "okay";
    };

    &uart1 {
    pinctrl-names = "default";
    pinctrl-0 = <&uart1_pins>;

    status = "okay";
    };

    &i2c0 {
    pinctrl-names = "default";
    pinctrl-0 = <&i2c0_pins>;

    status = "okay";
    clock-frequency = <100000>;
    };

    &i2c1 {
    pinctrl-names = "default";
    pinctrl-0 = <&i2c1_pins>;

    status = "okay";
    clock-frequency = <100000>;

    };


    &elm {
    status = "okay";
    };


    &gpmc {
    status = "okay";
    pinctrl-names = "default";
    pinctrl-0 = <&nandflash_pins_s0>;
    ranges = <0 0 0x10000000 0x10000000>; /* CS0: 16MB for NAND */
    nand@0,0 {
    compatible = "ti,omap2-nand";
    reg = <0 0 0x1000000>; /* CS0, offset 0, size 16MB or the TI code in omap-gpmc.c will screw up! */
    ti,nand-ecc-opt = "bch8";
    ti,elm-id = <&elm>;
    nand-bus-width = <8>;
    gpmc,time-para-granularity = <1>;
    gpmc,device-width = <1>;
    gpmc,burst-width = <0>;
    gpmc,burst-wrap = <0>;
    gpmc,sync-clk-ps = <40000>; /* converted to ps */
    gpmc,cs-on-ns = <0>;
    gpmc,cs-rd-off-ns = <300>; /* values are 10x higher (from standalone where it is in ticks) */
    gpmc,cs-wr-off-ns = <100>; /* as they are later divided using clock rate formula */
    gpmc,adv-on-ns = <0>;
    gpmc,adv-rd-off-ns = <100>;
    gpmc,adv-wr-off-ns = <100>;
    gpmc,we-on-ns = <0>;
    gpmc,we-off-ns = <50>;
    gpmc,oe-on-ns = <0>;
    gpmc,oe-off-ns = <100>;
    gpmc,access-ns = <110>;
    gpmc,rd-cycle-ns = <300>;
    gpmc,wr-cycle-ns = <100>;
    gpmc,bus-turnaround-ns = <0>;
    gpmc,cycle2cycle-delay-ns = <0>;
    gpmc,clk-activation-ns = <0>;
    gpmc,wr-access-ns = <0>;
    gpmc,wr-data-mux-bus-ns = <0>;
    /* MTD partition table */
    #address-cells = <1>;
    #size-cells = <1>;
    partition@0 {
    label = "boot";
    reg = <0x00000000 0x08000000>;
    };
    partition@1 {
    label = "root";
    reg = <0x08000000 0x78000000>;
    };
    };
    };


    &usb {
    status = "okay";
    };

    &usb_ctrl_mod {
    status = "okay";
    };

    &usb0_phy {
    status = "okay";
    };

    &usb1_phy {
    status = "okay";
    };

    &usb0 {
    status = "okay";
    };

    &usb0 {
    status = "okay";
    dr_mode = "host";
    };

    &usb1 {
    status = "okay";
    dr_mode = "host";
    };

    &cppi41dma {
    status = "okay";
    };

     

  • Are you still having problems?

    Steve K.