Part Number: PROCESSOR-SDK-AM437X
Tool/software: Linux
Hi
we have a custom board based on AM437X evm. The board has SPI boot options. For booting we have to copy MLO.byteswap into SPI flash and it takes u-boot.img and rootfs from eMMC . we had it working in u-boot 2016 in linux SDK 03.00.00.04
we are using winbond,w25x20 SPI flash.
Now we have ported with similar changes to latest SDK ti-processor-sdk-linux-am437x-evm-04.02.00.09 But here SPI boot is not working properly . we are facing following errors
U-Boot SPL 2017.01-00465-g4ff3d12-dirty (Mar 08 2018 - 13:03:13)
Trying to boot from SPI
Invalid bus 0 (err=-19)
SPI probe failed.
SPL: failed to boot from all boot devices
### ERROR ### Please RESET the board ###
Any idea why there is such errors and what could be the reason?
Regards,
Pavan S