Part Number: PROCESSOR-SDK-AM335X
Tool/software: Linux
Hi,
Cannot Enable MMC-2 , Below are my details,
Kernel Log :
root@txsky:~# dmesg | grep "4781000"
[ 1.546007] omap_hsmmc 47810000.mmc: GPIO lookup for consumer cd
[ 1.546019] omap_hsmmc 47810000.mmc: using device tree for GPIO lookup
[ 1.546031] of_get_named_gpiod_flags: can't parse 'cd-gpios' property of node '/ocp/mmc@47810000[0]'
[ 1.546038] of_get_named_gpiod_flags: can't parse 'cd-gpio' property of node '/ocp/mmc@47810000[0]'
[ 1.546043] omap_hsmmc 47810000.mmc: using lookup tables for GPIO lookup
[ 1.546050] omap_hsmmc 47810000.mmc: lookup for GPIO cd failed
[ 1.546058] omap_hsmmc 47810000.mmc: GPIO lookup for consumer wp
[ 1.546064] omap_hsmmc 47810000.mmc: using device tree for GPIO lookup
[ 1.546070] of_get_named_gpiod_flags: can't parse 'wp-gpios' property of node '/ocp/mmc@47810000[0]'
[ 1.546077] of_get_named_gpiod_flags: can't parse 'wp-gpio' property of node '/ocp/mmc@47810000[0]'
[ 1.546083] omap_hsmmc 47810000.mmc: using lookup tables for GPIO lookup
[ 1.546090] omap_hsmmc 47810000.mmc: lookup for GPIO wp failed
[ 1.546304] OF: /ocp/mmc@47810000: could not get #dma-cells for /ocp/l4_wkup@44c00000/prcm@200000/clocks/sysclkout_pre_ck@700
[ 1.557766] omap_hsmmc 47810000.mmc: RX DMA channel request failed
root@txsky:~#
DTS :
&mmc3 {
/* these are on the crossbar and are outlined in the
xbar-event-map element */
dmas = <&edma 30
&edma 31>;
dma-names = "tx", "rx";
status = "okay";
enable-sdio-wakeup;
vmmc-supply = <&wlan_en_reg>;
bus-width = <4>;
pinctrl-names = "default";
pinctrl-0 = <&mmc2_pins &wlan_pins>;
ti,non-removable;
ti,needs-special-hs-handling;
cap-power-off-card;
keep-power-in-suspend;
};
I tried with the following DMA configurations also,
dmas = <&edma 12
&edma 13>;
But its not Working. Please help me to resolve this issue .