Part Number: TMS320C6472
Tool/software: TI-RTOS
Hello,
I have a set of XDC modules which were developed for the C6472, and would like to compile them for functional testing under Linux.
I have attempted to mimic the example from the RTSC-Pedia:
rtsc.eclipse.org/.../Consuming_Configurable_Content
rtsc.eclipse.org/.../makefiles
When running make I get the following error message:
/home/domain/borton/Perforce/tidsp/ti_rtsc/bios_6_52_00_12/packages/gnu/targets/rts86U/lib/gnu.targets.rts86U.a86_64U(Error.o86_64U): In function `xdc_runtime_Error_policyMin__E':
Error.c:(.text.xdc_runtime_Error_policyMin__E+0x16): undefined reference to `xdc_runtime_Error_IgnoreBlock'
/home/domain/borton/Perforce/tidsp/ti_rtsc/bios_6_52_00_12/packages/gnu/targets/rts86U/lib/gnu.targets.rts86U.a86_64U(Error.o86_64U): In function `xdc_runtime_Error_init__E':
Error.c:(.text.xdc_runtime_Error_init__E+0x8): undefined reference to `xdc_runtime_Error_IgnoreBlock'
collect2: error: ld returned 1 exit status
I am running xdctools_3_32_01_22_core