Part Number: DM3730
Tool/software: Linux
Hi Everyone,
What this line means while booting DM3730 -> At line 3011 of func nand_scan_tail in file nand_base.c ?
can anyone say what is the problem while it shows following error during nand whole chip erase?
NAND erase.chip: device 0 whole chip
Skipping bad block at 0x00000000
Skipping bad block at 0x00010000
Skipping bad block at 0x00020000
Skipping bad block at 0x00030000
Skipping bad block at 0x00040000
Skipping bad block at 0x00060000
Skipping bad block at 0x00070000
Skipping bad block at 0x00080000
Skipping bad block at 0x00090000
Skipping bad block at 0x10000000
Skipping bad block at 0x10010000
Skipping bad block at 0x10020000
Skipping bad block at 0x10030000
Skipping bad block at 0x10040000
Skipping bad block at 0x10060000
Skipping bad block at 0x10070000
Skipping bad block at 0x10080000
Skipping bad block at 0x10090000
Skipping bad block at 0x20000000
Skipping bad block at 0x20010000
Skipping bad block at 0x20020000
Skipping bad block at 0x20030000
Skipping bad block at 0x20040000
Skipping bad block at 0x20060000
Skipping bad block at 0x20070000
Skipping bad block at 0x20080000
Skipping bad block at 0x20090000
Skipping bad block at 0x30000000
Skipping bad block at 0x30010000
Skipping bad block at 0x30020000
Skipping bad block at 0x30030000
Skipping bad block at 0x30040000
Skipping bad block at 0x30060000
Skipping bad block at 0x30070000
Skipping bad block at 0x30080000
Skipping bad block at 0x30090000
Erasing at 0x3fff0000 -- 100% complete.
Ok
Thanks & Regards,
M.Arun kumar