This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/EVMK2H: ti-processor-sdk-linux-k2hk-evm-04.02.00.09-Linux-x86-Install.bin Syntax error: Unterminated quoted string

Part Number: EVMK2H

Tool/software: Linux

Hello all,

I have a EVMK2H processor eval board that lost it's boot code (stored in the peripheral NOR Flash). I have attempted to install the subject SDK in order to reload the NOR Flash boot code and am getting the subject error (Syntax error: Unterminated quoted string). I have double checked version (running 64-bit Linux with Ubunutu 16.04 LTS). 

I followed the install procedure in the installer guide as follows:

Input: chmod +x ./ti-processor-sdk-linux-k2hk-evm-04.02.00.09-Linux-x86-Install.bin

Input: sudo ./ti-processor-sdk-linux-k2hk-evm-04.02.00.09-Linux-x86-Install.bin

Result: ./ti-processor-sdk-linux-k2hk-evm-04.02.00.09-Linux-x86-Install.bin: 1: ./ti-processor-sdk-linux-k2hk-evm-04.02.00.09-Linux-x86-Install.bin: Syntax error: Unterminated quoted string

Input: uname -m

Result: x86_64

Input: lsb_release -a

Result: 

No LSB modules are available.
Distributor ID: Ubuntu
Description: Ubuntu 16.04.3 LTS
Release: 16.04
Codename: xenial

Not sure what else to try and any help would be appreciated.