This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/RFSDK: sys/bios

Part Number: RFSDK
Other Parts Discussed in Thread: TCI6630K2L, 66AK2L06

Tool/software: Linux

hello expert,

I am a novice.I want to ask whether I can use the RFSDK in the sys/bios.I used to develop the program in windows.I read the installation guide.There need the u-boot.Could you give me some useful imformation to make a decision it is more Convenient and quick to develop the RFSDK in windows and linux?

Regards,

  • Which RFSDK version is this?
  • https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/run_5F00_lm_5F00_lte20FDD_5F00_RFtest1.shHello,

    RFSDK is a set of ARM software to control peripherals for TCI6630K2L or 66AK2L06 SOC processors.  The external control of the RFSDK can be done over standard Linux terminals using RS232 or Telnet-Ethernet connections, with shell scripts.  There is also an external HTML webpage described in the User Guide for control.  

    There is not a provision for PC control.  Although the messages needed would mimic sending messages to the RFSDK daemon in Linux.

    An example script is attached.

    Regards,

    Joe Quintal