This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TDA2SX: PCIe, SATA and USB simultaneously

Part Number: TDA2SX

Tool/software: Linux

Hello all,

We are using TDA2xx, and would like to use PCIe, SATA and USB interfaces. 

In the documentation, we have seen that SATA is only supported under Linux+BIOS configuration, not in RTOS only configuration.

Are there any limits/issues when using these three (PCIe, SATA and USB) at the same time compared to the single usage of only one of them? 

Thanks in advance,

Milena

  • hi
    Yes, You can have all these interfaces at the same time with VSDK Linux configuration where A15 running Linux control all these peripherals. Please check the pinMux configuration and make sure any of your other devices do not share same pins of these interfaces

    regards, Shiju