Part Number: TDA2PXEVM
Tool/software: TI-RTOS
Hi
We are working for a system based on TDA2px . The system will be BIOS only. The PDK being used is PROCESSOR_SDK_VISION_03_02_00_00
As I understand the sample example ..\PROCESSOR_SDK_VISION_03_02_00_00\ti_components\drivers\pdk_01_08_01_06\packages\ti\drv\stw_lld\examples\mmcsd\sd_file_io
deals with SD card file system read write test running from IPU core.(from make file provided in the same example)
Please let me know if this is correct and if SD card can be accessed from other cores for file read/write operations.
This feature is needed along with ability to boot from SD Card.
regards
Hrishikesh