This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Compiler/TDA3MV: ISS Capture Link Output Data Format

Part Number: TDA3MV

Tool/software: TI C/C++ Compiler

Hi, 

Our usecase is using the ISS Capture Link, along with the OV10640 IMI sensor, in TDA3X .

We got the following error while changing the output data format of the ISS Capture Link to SYSTEM_DF_YUV422I_YUYV :


Assertion @ Line: 165 in issM2mIspLink_drv_apply_config.c: status == FVID2_SOK : failed !!!

Does the ISS Capture Link support SYSTEM_DF_YUV422I_YUYV as its output format ??

An early response from your side will be highly appreciated.

Regards,
Khilav Soni