Other Parts Discussed in Thread: OMAP3530, TPS65920, TPS65950
Hi,
we have a custom OMAP3530 board, very similar to the beagleboard, using the TPS65920 power-companion instead of TPS65950.
Some times when we apply power to the board the OMAP3530 gets stuck and doesn't try to boot from either NAND, serial or USB, and it doesn't release nSYS_RESWARM.
To me this suggests that the bootrom is not executing (JTAG probe is on the way...)
Both 32khz and 26 MHz clock and all power-rails are working and the nSYS_RESPWRON from TPS65920 is released and is fine, when this occurs.
Re-powering OR activating a cold-reset (pulling nSYS_RESPWRON to GND) unfreezes the OMAP3530 and then it boots just fine (from either of the interfaces).
Any hints on where to look for something which can inflict this damage? As far as I understand, the TPS65920 should guarantee the correct power-sequencing and keeping nSYS_RESPWRON until the power is stable.
This seems to occur only on the second of our two first batches of boards, so there is a possibility that any of the components for example a capacitor is mounted incorrectly by the manufacturer, something which is quite difficult to troubleshoot of course..
Thanks for any hints anyway,
regards,
Bjorn