Other Parts Discussed in Thread: AM3358
Hello community,
I have a custom board with AM3358 similar with the BBB but without HDMI and without eMMC. I copied the layout from the DDR3 but I use the MT41K256M16TW-107 and not the MT41K512M16HA-125.
I've tried to bring up the board and calculate the DDR values and add them to the ddr_defs.h. After enter "#define DEBUG" to the file ti_am335x_common.h, I see that the bootup stops at the DDR. To find the mistake, I added printf to the file board/ti/am335x/board.c , but they never show in the terminal. Because of this, I have a few questions:
1. Did somebody bring up a AM3358 with MT41K256M16TW-107 and could share the calculated values?
2. I used these commands to build the u-boot:
- make CROSS_COMPILE=arm-linux-gnueabihf- distclean
- make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- am335x_boneblack_defconfig
- make CROSS_COMPILE=arm-linux-gnueabihf- -j4
Why can't I see the printf from board.c during the bootup? Is this file not used in the u-boot?
3. It seems to me that the file ddr_defs.h is not the right file to set the ddr values for the u-boot. Could someone confirm this?
Thank you for your help.
I attache the ddr_configuration, ddr_defs.h, board.c and the output from the bootup
best regards
eric
AM335x_DDR_register_calc_tool_new.xlslog_am335x.txt1452.ddr_defs.h
/*
* board.c
*
* Board functions for TI AM335X based boards
*
* Copyright (C) 2011, Texas Instruments, Incorporated - http://www.ti.com/
*
* SPDX-License-Identifier: GPL-2.0+
*/
#include <common.h>
#include <dm.h>
#include <errno.h>
#include <spl.h>
#include <serial.h>
#include <asm/arch/cpu.h>
#include <asm/arch/hardware.h>
#include <asm/arch/omap.h>
#include <asm/arch/ddr_defs.h>
#include <asm/arch/clock.h>
#include <asm/arch/clk_synthesizer.h>
#include <asm/arch/gpio.h>
#include <asm/arch/mmc_host_def.h>
#include <asm/arch/sys_proto.h>
#include <asm/arch/mem.h>
#include <asm/io.h>
#include <asm/emif.h>
#include <asm/gpio.h>
#include <asm/omap_common.h>
#include <asm/omap_sec_common.h>
#include <asm/omap_mmc.h>
#include <i2c.h>
#include <miiphy.h>
#include <cpsw.h>
#include <power/tps65217.h>
#include <power/tps65910.h>
#include <environment.h>
#include <watchdog.h>
#include <environment.h>
#include "../common/board_detect.h"
#include "board.h"
#include "hash-string.h"
DECLARE_GLOBAL_DATA_PTR;
/* GPIO that controls power to DDR on EVM-SK */
#define GPIO_TO_PIN(bank, gpio) (32 * (bank) + (gpio))
#define GPIO_DDR_VTT_EN GPIO_TO_PIN(0, 7)
#define ICE_GPIO_DDR_VTT_EN GPIO_TO_PIN(0, 18)
#define GPIO_PR1_MII_CTRL GPIO_TO_PIN(3, 4)
#define GPIO_MUX_MII_CTRL GPIO_TO_PIN(3, 10)
#define GPIO_FET_SWITCH_CTRL GPIO_TO_PIN(0, 7)
#define GPIO_PHY_RESET GPIO_TO_PIN(2, 5)
#define GPIO_ETH0_MODE GPIO_TO_PIN(0, 11)
#define GPIO_ETH1_MODE GPIO_TO_PIN(1, 26)
static struct ctrl_dev *cdev = (struct ctrl_dev *)CTRL_DEVICE_BASE;
#define GPIO0_RISINGDETECT (AM33XX_GPIO0_BASE + OMAP_GPIO_RISINGDETECT)
#define GPIO1_RISINGDETECT (AM33XX_GPIO1_BASE + OMAP_GPIO_RISINGDETECT)
#define GPIO0_IRQSTATUS1 (AM33XX_GPIO0_BASE + OMAP_GPIO_IRQSTATUS1)
#define GPIO1_IRQSTATUS1 (AM33XX_GPIO1_BASE + OMAP_GPIO_IRQSTATUS1)
#define GPIO0_IRQSTATUSRAW (AM33XX_GPIO0_BASE + 0x024)
#define GPIO1_IRQSTATUSRAW (AM33XX_GPIO1_BASE + 0x024)
/*
* Read header information from EEPROM into global structure.
*/
#ifdef CONFIG_TI_I2C_BOARD_DETECT
void do_board_detect(void)
{
enable_i2c0_pin_mux();
i2c_init(CONFIG_SYS_OMAP24_I2C_SPEED, CONFIG_SYS_OMAP24_I2C_SLAVE);
if (ti_i2c_eeprom_am_get(CONFIG_EEPROM_BUS_ADDRESS,
CONFIG_EEPROM_CHIP_ADDRESS))
printf("ti_i2c_eeprom_init failed\n");
//hack-ish, needs to mux'ed early, in do_cape_detect was too late...
enable_i2c2_pin_mux();
i2c_init(CONFIG_SYS_OMAP24_I2C_SPEED2, CONFIG_SYS_OMAP24_I2C_SLAVE2);
}
#endif
#define CAPE_EEPROM_ADDR0 0x54
#define CAPE_EEPROM_ADDR1 0x55
#define CAPE_EEPROM_ADDR2 0x56
#define CAPE_EEPROM_ADDR3 0x57
void write_hex (unsigned char i)
{
char cc;
cc = i >> 4;
cc &= 0xf;
if (cc > 9)
serial_putc (cc + 55);
else
serial_putc (cc + 48);
cc = i & 0xf;
if (cc > 9)
serial_putc (cc + 55);
else
serial_putc (cc + 48);
}
#define NOT_POP 0x0
#define PINS_TAKEN 0x0
#define UNK_BASE_DTB 0x0
#define BB_BASE_DTB 0x1
#define BBB_BASE_DTB 0x2
#define BBBL_BASE_DTB 0x3
#define BBE_BASE_DTB 0x4
#define BBB_EMMC 0x1
#define BBB_TDA998X_AUDIO 0x1
#define BBB_TDA998X_NAUDIO 0x2
#define BBB_ADV7511_AUDIO 0x3
#define BBB_ADV7511_NAUDIO 0x4
#define BBB_ADC 0x1
#define BBBW_WL1835 0x1
#define BBGW_WL1835 0x2
#define CAPE_UNIVERSAL 0x0
#define CAPE_UNIVERSAL_BBB 0x01
#define CAPE_UNIVERSAL_BBG 0x02
#define CAPE_UNIVERSAL_BBGW 0x03
#define M_BBG1 0x01
#define M_OS00 0x02
static int probe_cape_eeprom(struct am335x_cape_eeprom_id *cape_header)
{
unsigned char addr;
/* /lib/firmware/BB-CAPE-DISP-CT4-00A0.dtbo */
/* 14 + 16 + 1 + 4 + 5 = 40 */
char cape_overlay[40];
char process_cape_part_number[16];
char end_part_number;
char cape_overlay_pass_to_kernel[18];
//Don't forget about the BeagleBone Classic (White)
char base_dtb=UNK_BASE_DTB;
char virtual_emmc=NOT_POP;
char virtual_video=NOT_POP;
char virtual_audio=NOT_POP;
char virtual_wireless=NOT_POP;
char cape_universal=CAPE_UNIVERSAL;
char virtual_adc=NOT_POP;
char model=NOT_POP;
char *name = NULL;
if (board_is_bone_lt()) {
puts("BeagleBone Black:\n");
base_dtb=BBB_BASE_DTB;
virtual_emmc=BBB_EMMC;
virtual_video=BBB_TDA998X_AUDIO;
virtual_audio=BBB_TDA998X_AUDIO;
virtual_wireless=NOT_POP;
virtual_adc=BBB_ADC;
cape_universal=CAPE_UNIVERSAL_BBB;
name = "A335BNLT";
if (!strncmp(board_ti_get_rev(), "BLA", 3)) {
puts("Model: BeagleBoard.org BeagleBone Blue:\n");
/* Special case */
base_dtb=BBBL_BASE_DTB;
virtual_emmc=NOT_POP;
virtual_video=NOT_POP;
virtual_audio=NOT_POP;
virtual_wireless=NOT_POP;
virtual_adc=BBB_ADC;
cape_universal=CAPE_UNIVERSAL;
name = "BBBL";
}
if (!strncmp(board_ti_get_rev(), "BW", 2)) {
puts("Model: BeagleBoard.org BeagleBone Black Wireless:\n");
virtual_wireless=BBBW_WL1835;
name = "BBBW";
}
if (!strncmp(board_ti_get_rev(), "BBG", 3)) {
/* catches again in board_is_bbg1() */
//puts("Model: SeeedStudio BeagleBone Green:\n");
virtual_video=NOT_POP;
virtual_audio=NOT_POP;
cape_universal=CAPE_UNIVERSAL_BBG;
name = "BBG1";
model=M_BBG1;
}
if (!strncmp(board_ti_get_rev(), "GW1", 3)) {
puts("Model: SeeedStudio BeagleBone Green Wireless:\n");
virtual_video=NOT_POP;
virtual_audio=NOT_POP;
virtual_wireless=BBGW_WL1835;
cape_universal=CAPE_UNIVERSAL_BBGW;
}
if (!strncmp(board_ti_get_rev(), "AIA", 3)) {
puts("Model: Arrow BeagleBone Black Industrial:\n");
virtual_video=BBB_ADV7511_AUDIO;
virtual_audio=BBB_ADV7511_AUDIO;
cape_universal=CAPE_UNIVERSAL;
}
if (!strncmp(board_ti_get_rev(), "EIA", 3)) {
puts("Model: Element14 BeagleBone Black Industrial:\n");
}
if (!strncmp(board_ti_get_rev(), "SE", 2)) {
puts("Model: SanCloud BeagleBone Enhanced:\n");
base_dtb=BBE_BASE_DTB;
cape_universal=CAPE_UNIVERSAL_BBB;
name = "SBBE";
}
if (!strncmp(board_ti_get_rev(), "ME0", 3)) {
puts("Model: MENTOREL BeagleBone uSomIQ:\n");
virtual_video=NOT_POP;
virtual_audio=NOT_POP;
cape_universal=CAPE_UNIVERSAL_BBG;
}
if (!strncmp(board_ti_get_rev(), "NAD", 3)) {
puts("Model: Neuromeka BeagleBone Air:\n");
cape_universal=CAPE_UNIVERSAL;
}
if (!strncmp(board_ti_get_rev(), "OS0", 3)) {
puts("Model: Octavo Systems OSD3358-SM-RED:\n");
name = "OS00";
cape_universal=NOT_POP;
model=M_OS00;
}
}
if (board_is_bone()) {
puts("Model: BeagleBone:\n");
base_dtb=BB_BASE_DTB;
virtual_emmc=NOT_POP;
virtual_video=NOT_POP;
virtual_audio=NOT_POP;
virtual_wireless=NOT_POP;
virtual_adc=BBB_ADC;
cape_universal=CAPE_UNIVERSAL_BBB;
name = "A335BONE";
}
if (board_is_bbg1()) {
puts("Model: SeeedStudio BeagleBone Green:\n");
base_dtb=BBB_BASE_DTB;
virtual_emmc=BBB_EMMC;
virtual_video=NOT_POP;
virtual_audio=NOT_POP;
virtual_wireless=NOT_POP;
virtual_adc=BBB_ADC;
cape_universal=CAPE_UNIVERSAL_BBG;
name = "BBG1";
model=M_BBG1;
}
set_board_info_env(name);
i2c_set_bus_num(2);
strlcpy(cape_overlay_pass_to_kernel, "", 1);
for ( addr = CAPE_EEPROM_ADDR0; addr <= CAPE_EEPROM_ADDR3; addr++ ) {
if (i2c_probe(addr)) {
puts("BeagleBone: cape eeprom: i2c_probe: 0x"); write_hex(addr); puts(":\n");
} else {
/* read the eeprom using i2c */
if (i2c_read(addr, 0, 2, (uchar *)cape_header,
sizeof(struct am335x_cape_eeprom_id))) {
puts("BeagleBone: cape eeprom: Could not read the EEPROM; something fundamentally"
" wrong on the I2C bus.\n");
return -EIO;
}
if (cape_header->header == 0xEE3355AA) {
strlcpy(cape_overlay, "/lib/firmware/", 14 + 1);
strlcpy(cape_overlay_pass_to_kernel, "", 2);
strlcpy(process_cape_part_number, "...............", 16 + 1);
strlcpy(process_cape_part_number, cape_header->part_number, 16 + 1);
printf("debug: process_cape_part_number:[%s]\n", process_cape_part_number);
//FIXME: some capes end with '.'
if ( process_cape_part_number[15] == 0x2E ) {
puts("debug: fixup, extra . in eeprom field\n");
process_cape_part_number[15] = 0x00;
if ( process_cape_part_number[14] == 0x2E ) {
process_cape_part_number[14] = 0x00;
}
}
//Find ending 0x00
puts("debug: process_cape_part_number:[");
end_part_number=16;
for ( int i=0; i <= 16; i++ ) {
if ( process_cape_part_number[i] == 0x00 ) {
end_part_number=i;
i=17;
} else {
write_hex(process_cape_part_number[i]);
}
}
puts("]\n");
strncat(cape_overlay, process_cape_part_number, end_part_number);
//printf("debug: %s\n", cape_overlay);
strncat(cape_overlay, "-", 1);
//printf("debug: %s\n", cape_overlay);
strncat(cape_overlay, cape_header->version, 4);
//printf("debug: %s\n", cape_overlay);
strncat(cape_overlay, ".dtbo", 5);
//printf("debug: %s\n", cape_overlay);
unsigned long cape_overlay_hash = hash_string(cape_overlay);
puts("BeagleBone: cape eeprom: i2c_probe: 0x");
write_hex(addr);
printf(": %s [0x%lx]\n", cape_overlay, cape_overlay_hash);
strncat(cape_overlay_pass_to_kernel, process_cape_part_number, end_part_number);
strncat(cape_overlay_pass_to_kernel, ",", 1);
switch(cape_overlay_hash) {
case 0x3c766f: /* /lib/firmware/BB-CAPE-DISP-CT4-00A0.dtbo */
virtual_video=PINS_TAKEN;
break;
case 0x24f51cf: /* /lib/firmware/BB-BONE-CAM-VVDN-00A0.dtbo */
virtual_emmc=PINS_TAKEN;
break;
case 0x4b0c13f: /* /lib/firmware/NL-AB-BBCL-00B0.dtbo */
virtual_video=PINS_TAKEN;
break;
case 0x74e7bbf: /* /lib/firmware/bb-justboom-dac-00A0.dtbo */
virtual_audio=PINS_TAKEN;
break;
case 0x93b574f: /* /lib/firmware/BB-GREEN-HDMI-00A0.dtbo */
virtual_video=PINS_TAKEN;
break;
case 0xb1b7bbf: /* /lib/firmware/bb-justboom-amp-00A0.dtbo */
virtual_audio=PINS_TAKEN;
break;
//d15bb
case 0xd15b80f: /* /lib/firmware/DLPDLCR2000-00A0.dtbo */
virtual_video=PINS_TAKEN;
break;
case 0xd4c9eff: /* /lib/firmware/bb-justboom-digi-00A0.dtbo */
virtual_audio=PINS_TAKEN;
break;
case 0xe3f55df: /* /lib/firmware/BB-BONE-NH7C-01-A0.dtbo */
virtual_video=PINS_TAKEN;
break;
case 0xfc93c8f: /* /lib/firmware/BB-BONE-LCD7-01-00A3.dtbo */
virtual_video=PINS_TAKEN;
virtual_adc=PINS_TAKEN;
break;
//fe131
case 0xfe1313f: /* /lib/firmware/BB-BONE-4D5R-01-00A1.dtbo */
virtual_video=PINS_TAKEN;
break;
//fe132
case 0xfe1323f: /* /lib/firmware/BB-BONE-4D4R-01-00A1.dtbo */
virtual_video=PINS_TAKEN;
break;
case 0xfe1327f: /* /lib/firmware/BB-BONE-4D4N-01-00A1.dtbo */
virtual_video=PINS_TAKEN;
break;
case 0xfe132cf: /* /lib/firmware/BB-BONE-4D4C-01-00A1.dtbo */
virtual_video=PINS_TAKEN;
break;
//fe133
case 0xfe1337f: /* /lib/firmware/BB-BONE-4D7N-01-00A1.dtbo */
virtual_video=PINS_TAKEN;
break;
case 0xfe133cf: /* /lib/firmware/BB-BONE-4D7C-01-00A1.dtbo */
virtual_video=PINS_TAKEN;
break;
//fe135
case 0xfe1357f: /* /lib/firmware/BB-BONE-4D5N-01-00A1.dtbo */
virtual_video=PINS_TAKEN;
break;
case 0xfe135cf: /* /lib/firmware/BB-BONE-4D5C-01-00A1.dtbo */
virtual_video=PINS_TAKEN;
break;
//fe137
case 0xfe1373f: /* /lib/firmware/BB-BONE-4D7R-01-00A1.dtbo */
virtual_video=PINS_TAKEN;
break;
case 0xfe93c1f: /* /lib/firmware/BB-BONE-LCD4-01-00A1.dtbo */
virtual_video=PINS_TAKEN;
virtual_adc=PINS_TAKEN;
break;
}
switch(addr) {
case CAPE_EEPROM_ADDR0:
env_set("uboot_overlay_addr0", cape_overlay);
env_set("uboot_detected_capes_addr0", cape_overlay_pass_to_kernel);
break;
case CAPE_EEPROM_ADDR1:
env_set("uboot_overlay_addr1", cape_overlay);
env_set("uboot_detected_capes_addr1", cape_overlay_pass_to_kernel);
break;
case CAPE_EEPROM_ADDR2:
env_set("uboot_overlay_addr2", cape_overlay);
env_set("uboot_detected_capes_addr2", cape_overlay_pass_to_kernel);
break;
case CAPE_EEPROM_ADDR3:
env_set("uboot_overlay_addr3", cape_overlay);
env_set("uboot_detected_capes_addr3", cape_overlay_pass_to_kernel);
break;
}
env_set("uboot_detected_capes", "1");
} else {
puts("BeagleBone: found invalid cape eeprom: i2c_probe: 0x"); write_hex(addr); puts(":\n");
}
}
}//for
switch(base_dtb) {
case BB_BASE_DTB:
env_set("uboot_base_dtb", "am335x-bone.dtb");
env_set("uboot_try_cape_universal", "1");
break;
case BBB_BASE_DTB:
env_set("uboot_base_dtb", "am335x-boneblack-uboot.dtb");
env_set("uboot_try_cape_universal", "1");
break;
case BBE_BASE_DTB:
env_set("uboot_base_dtb", "am335x-sancloud-bbe-uboot.dtb");
env_set("uboot_try_cape_universal", "1");
break;
case BBBL_BASE_DTB:
env_set("uboot_base_dtb", "am335x-boneblue.dtb");
break;
}
if (virtual_emmc == BBB_EMMC) {
env_set("uboot_emmc", "/lib/firmware/BB-BONE-eMMC1-01-00A0.dtbo");
}
switch(virtual_video) {
case BBB_TDA998X_AUDIO:
if (virtual_audio == PINS_TAKEN) {
env_set("uboot_video", "/lib/firmware/BB-NHDMI-TDA998x-00A0.dtbo");
env_set("uboot_video_naudio", "/lib/firmware/BB-NHDMI-TDA998x-00A0.dtbo");
} else {
env_set("uboot_video", "/lib/firmware/BB-HDMI-TDA998x-00A0.dtbo");
env_set("uboot_video_naudio", "/lib/firmware/BB-NHDMI-TDA998x-00A0.dtbo");
}
break;
case BBB_TDA998X_NAUDIO:
env_set("uboot_video", "/lib/firmware/BB-NHDMI-TDA998x-00A0.dtbo");
env_set("uboot_video_naudio", "/lib/firmware/BB-NHDMI-TDA998x-00A0.dtbo");
break;
case BBB_ADV7511_AUDIO:
if (virtual_audio == PINS_TAKEN) {
env_set("uboot_video", "/lib/firmware/BB-NHDMI-ADV7511-00A0.dtbo");
env_set("uboot_video_naudio", "/lib/firmware/BB-NHDMI-ADV7511-00A0.dtbo");
} else {
env_set("uboot_video", "/lib/firmware/BB-HDMI-ADV7511-00A0.dtbo");
env_set("uboot_video_naudio", "/lib/firmware/BB-NHDMI-ADV7511-00A0.dtbo");
}
break;
case BBB_ADV7511_NAUDIO:
env_set("uboot_video", "/lib/firmware/BB-NHDMI-ADV7511-00A0.dtbo");
env_set("uboot_video_naudio", "/lib/firmware/BB-NHDMI-ADV7511-00A0.dtbo");
break;
}
switch(virtual_wireless) {
case BBBW_WL1835:
env_set("uboot_wireless", "/lib/firmware/BB-BBBW-WL1835-00A0.dtbo");
break;
case BBGW_WL1835:
env_set("uboot_wireless", "/lib/firmware/BB-BBGW-WL1835-00A0.dtbo");
break;
}
switch(virtual_adc) {
case BBB_ADC:
env_set("uboot_adc", "/lib/firmware/BB-ADC-00A0.dtbo");
break;
}
switch(model) {
case M_BBG1:
env_set("uboot_model", "/lib/firmware/M-BB-BBG-00A0.dtbo");
break;
case M_OS00:
env_set("uboot_model", "/lib/firmware/M-BB-OSD3358-SM-RED-00A0.dtbo");
break;
}
switch(cape_universal) {
case CAPE_UNIVERSAL_BBB:
env_set("uboot_cape_universal_bbb", "1");
break;
case CAPE_UNIVERSAL_BBG:
env_set("uboot_cape_universal_bbg", "1");
break;
case CAPE_UNIVERSAL_BBGW:
env_set("uboot_cape_universal_bbgw", "1");
break;
}
i2c_set_bus_num(0);
return 0;
}
void do_cape_detect(void)
{
struct am335x_cape_eeprom_id cape_header;
i2c_init(CONFIG_SYS_OMAP24_I2C_SPEED2, CONFIG_SYS_OMAP24_I2C_SLAVE2);
probe_cape_eeprom(&cape_header);
}
#ifndef CONFIG_DM_SERIAL
struct serial_device *default_serial_console(void)
{
if (board_is_icev2())
return &eserial4_device;
else if (board_is_beaglelogic())
return &eserial5_device;
else
return &eserial1_device;
}
#endif
#ifndef CONFIG_SKIP_LOWLEVEL_INIT
static const struct ddr_data ddr2_data = {
.datardsratio0 = MT47H128M16RT25E_RD_DQS,
.datafwsratio0 = MT47H128M16RT25E_PHY_FIFO_WE,
.datawrsratio0 = MT47H128M16RT25E_PHY_WR_DATA,
};
static const struct cmd_control ddr2_cmd_ctrl_data = {
.cmd0csratio = MT47H128M16RT25E_RATIO,
.cmd1csratio = MT47H128M16RT25E_RATIO,
.cmd2csratio = MT47H128M16RT25E_RATIO,
};
static const struct emif_regs ddr2_emif_reg_data = {
.sdram_config = MT47H128M16RT25E_EMIF_SDCFG,
.ref_ctrl = MT47H128M16RT25E_EMIF_SDREF,
.sdram_tim1 = MT47H128M16RT25E_EMIF_TIM1,
.sdram_tim2 = MT47H128M16RT25E_EMIF_TIM2,
.sdram_tim3 = MT47H128M16RT25E_EMIF_TIM3,
.emif_ddr_phy_ctlr_1 = MT47H128M16RT25E_EMIF_READ_LATENCY,
};
static const struct emif_regs ddr2_evm_emif_reg_data = {
.sdram_config = MT47H128M16RT25E_EMIF_SDCFG,
.ref_ctrl = MT47H128M16RT25E_EMIF_SDREF,
.sdram_tim1 = MT47H128M16RT25E_EMIF_TIM1,
.sdram_tim2 = MT47H128M16RT25E_EMIF_TIM2,
.sdram_tim3 = MT47H128M16RT25E_EMIF_TIM3,
.ocp_config = EMIF_OCP_CONFIG_AM335X_EVM,
.emif_ddr_phy_ctlr_1 = MT47H128M16RT25E_EMIF_READ_LATENCY,
};
static const struct ddr_data ddr3_data = {
.datardsratio0 = MT41J128MJT125_RD_DQS,
.datawdsratio0 = MT41J128MJT125_WR_DQS,
.datafwsratio0 = MT41J128MJT125_PHY_FIFO_WE,
.datawrsratio0 = MT41J128MJT125_PHY_WR_DATA,
};
static const struct ddr_data ddr3_beagleblack_data = {
.datardsratio0 = MT41K256M16HA125E_RD_DQS,
.datawdsratio0 = MT41K256M16HA125E_WR_DQS,
.datafwsratio0 = MT41K256M16HA125E_PHY_FIFO_WE,
.datawrsratio0 = MT41K256M16HA125E_PHY_WR_DATA,
};
static const struct ddr_data ddr3_evm_data = {
.datardsratio0 = MT41J512M8RH125_RD_DQS,
.datawdsratio0 = MT41J512M8RH125_WR_DQS,
.datafwsratio0 = MT41J512M8RH125_PHY_FIFO_WE,
.datawrsratio0 = MT41J512M8RH125_PHY_WR_DATA,
};
static const struct ddr_data ddr3_icev2_data = {
.datardsratio0 = MT41J128MJT125_RD_DQS_400MHz,
.datawdsratio0 = MT41J128MJT125_WR_DQS_400MHz,
.datafwsratio0 = MT41J128MJT125_PHY_FIFO_WE_400MHz,
.datawrsratio0 = MT41J128MJT125_PHY_WR_DATA_400MHz,
};
static const struct cmd_control ddr3_cmd_ctrl_data = {
.cmd0csratio = MT41J128MJT125_RATIO,
.cmd0iclkout = MT41J128MJT125_INVERT_CLKOUT,
.cmd1csratio = MT41J128MJT125_RATIO,
.cmd1iclkout = MT41J128MJT125_INVERT_CLKOUT,
.cmd2csratio = MT41J128MJT125_RATIO,
.cmd2iclkout = MT41J128MJT125_INVERT_CLKOUT,
};
static const struct cmd_control ddr3_beagleblack_cmd_ctrl_data = {
.cmd0csratio = MT41K256M16HA125E_RATIO,
.cmd0iclkout = MT41K256M16HA125E_INVERT_CLKOUT,
.cmd1csratio = MT41K256M16HA125E_RATIO,
.cmd1iclkout = MT41K256M16HA125E_INVERT_CLKOUT,
.cmd2csratio = MT41K256M16HA125E_RATIO,
.cmd2iclkout = MT41K256M16HA125E_INVERT_CLKOUT,
};
static const struct cmd_control ddr3_evm_cmd_ctrl_data = {
.cmd0csratio = MT41J512M8RH125_RATIO,
.cmd0iclkout = MT41J512M8RH125_INVERT_CLKOUT,
.cmd1csratio = MT41J512M8RH125_RATIO,
.cmd1iclkout = MT41J512M8RH125_INVERT_CLKOUT,
.cmd2csratio = MT41J512M8RH125_RATIO,
.cmd2iclkout = MT41J512M8RH125_INVERT_CLKOUT,
};
static const struct cmd_control ddr3_icev2_cmd_ctrl_data = {
.cmd0csratio = MT41J128MJT125_RATIO_400MHz,
.cmd0iclkout = MT41J128MJT125_INVERT_CLKOUT_400MHz,
.cmd1csratio = MT41J128MJT125_RATIO_400MHz,
.cmd1iclkout = MT41J128MJT125_INVERT_CLKOUT_400MHz,
.cmd2csratio = MT41J128MJT125_RATIO_400MHz,
.cmd2iclkout = MT41J128MJT125_INVERT_CLKOUT_400MHz,
};
static struct emif_regs ddr3_emif_reg_data = {
.sdram_config = MT41J128MJT125_EMIF_SDCFG,
.ref_ctrl = MT41J128MJT125_EMIF_SDREF,
.sdram_tim1 = MT41J128MJT125_EMIF_TIM1,
.sdram_tim2 = MT41J128MJT125_EMIF_TIM2,
.sdram_tim3 = MT41J128MJT125_EMIF_TIM3,
.zq_config = MT41J128MJT125_ZQ_CFG,
.emif_ddr_phy_ctlr_1 = MT41J128MJT125_EMIF_READ_LATENCY |
PHY_EN_DYN_PWRDN,
};
static struct emif_regs ddr3_beagleblack_emif_reg_data = {
.sdram_config = MT41K256M16HA125E_EMIF_SDCFG,
.ref_ctrl = MT41K256M16HA125E_EMIF_SDREF,
.sdram_tim1 = MT41K256M16HA125E_EMIF_TIM1,
.sdram_tim2 = MT41K256M16HA125E_EMIF_TIM2,
.sdram_tim3 = MT41K256M16HA125E_EMIF_TIM3,
.ocp_config = EMIF_OCP_CONFIG_BEAGLEBONE_BLACK,
.zq_config = MT41K256M16HA125E_ZQ_CFG,
.emif_ddr_phy_ctlr_1 = MT41K256M16HA125E_EMIF_READ_LATENCY,
};
static struct emif_regs ddr3_evm_emif_reg_data = {
.sdram_config = MT41J512M8RH125_EMIF_SDCFG,
.ref_ctrl = MT41J512M8RH125_EMIF_SDREF,
.sdram_tim1 = MT41J512M8RH125_EMIF_TIM1,
.sdram_tim2 = MT41J512M8RH125_EMIF_TIM2,
.sdram_tim3 = MT41J512M8RH125_EMIF_TIM3,
.ocp_config = EMIF_OCP_CONFIG_AM335X_EVM,
.zq_config = MT41J512M8RH125_ZQ_CFG,
.emif_ddr_phy_ctlr_1 = MT41J512M8RH125_EMIF_READ_LATENCY |
PHY_EN_DYN_PWRDN,
};
static struct emif_regs ddr3_icev2_emif_reg_data = {
.sdram_config = MT41J128MJT125_EMIF_SDCFG_400MHz,
.ref_ctrl = MT41J128MJT125_EMIF_SDREF_400MHz,
.sdram_tim1 = MT41J128MJT125_EMIF_TIM1_400MHz,
.sdram_tim2 = MT41J128MJT125_EMIF_TIM2_400MHz,
.sdram_tim3 = MT41J128MJT125_EMIF_TIM3_400MHz,
.zq_config = MT41J128MJT125_ZQ_CFG_400MHz,
.emif_ddr_phy_ctlr_1 = MT41J128MJT125_EMIF_READ_LATENCY_400MHz |
PHY_EN_DYN_PWRDN,
};
#ifdef CONFIG_SPL_OS_BOOT
int spl_start_uboot(void)
{
/* break into full u-boot on 'c' */
if (serial_tstc() && serial_getc() == 'c')
return 1;
#ifdef CONFIG_SPL_ENV_SUPPORT
env_init();
env_load();
if (env_get_yesno("boot_os") != 1)
return 1;
#endif
return 0;
}
#endif
const struct dpll_params *get_dpll_ddr_params(void)
{
int ind = get_sys_clk_index();
if (board_is_evm_sk())
return &dpll_ddr3_303MHz[ind];
else if (board_is_pb() || board_is_bone_lt() || board_is_icev2() || board_is_beaglelogic())
return &dpll_ddr3_400MHz[ind];
else if (board_is_evm_15_or_later())
return &dpll_ddr3_303MHz[ind];
else
return &dpll_ddr2_266MHz[ind];
}
static u8 bone_not_connected_to_ac_power(void)
{
if (board_is_bone() && !board_is_pb()) {
uchar pmic_status_reg;
if (tps65217_reg_read(TPS65217_STATUS,
&pmic_status_reg))
return 1;
if (!(pmic_status_reg & TPS65217_PWR_SRC_AC_BITMASK)) {
puts("No AC power, switching to default OPP\n");
return 1;
}
}
return 0;
}
const struct dpll_params *get_dpll_mpu_params(void)
{
int ind = get_sys_clk_index();
int freq = am335x_get_efuse_mpu_max_freq(cdev);
if (bone_not_connected_to_ac_power())
freq = MPUPLL_M_600;
if (board_is_pb() || board_is_bone_lt() || board_is_beaglelogic())
freq = MPUPLL_M_1000;
switch (freq) {
case MPUPLL_M_1000:
return &dpll_mpu_opp[ind][5];
case MPUPLL_M_800:
return &dpll_mpu_opp[ind][4];
case MPUPLL_M_720:
return &dpll_mpu_opp[ind][3];
case MPUPLL_M_600:
return &dpll_mpu_opp[ind][2];
case MPUPLL_M_500:
return &dpll_mpu_opp100;
case MPUPLL_M_300:
return &dpll_mpu_opp[ind][0];
}
return &dpll_mpu_opp[ind][0];
}
static void scale_vcores_bone(int freq)
{
int usb_cur_lim, mpu_vdd;
/*
* Only perform PMIC configurations if board rev > A1
* on Beaglebone White
*/
if (!board_is_pb() && board_is_bone() && !strncmp(board_ti_get_rev(), "00A1", 4))
return;
if (i2c_probe(TPS65217_CHIP_PM))
return;
/*
* On Beaglebone White we need to ensure we have AC power
* before increasing the frequency.
*/
if (bone_not_connected_to_ac_power())
freq = MPUPLL_M_600;
/*
* Override what we have detected since we know if we have
* a Beaglebone Black it supports 1GHz.
*/
if (board_is_pb() || board_is_bone_lt() || board_is_beaglelogic())
freq = MPUPLL_M_1000;
switch (freq) {
case MPUPLL_M_1000:
mpu_vdd = TPS65217_DCDC_VOLT_SEL_1325MV;
usb_cur_lim = TPS65217_USB_INPUT_CUR_LIMIT_1800MA;
break;
case MPUPLL_M_800:
mpu_vdd = TPS65217_DCDC_VOLT_SEL_1275MV;
usb_cur_lim = TPS65217_USB_INPUT_CUR_LIMIT_1300MA;
break;
case MPUPLL_M_720:
mpu_vdd = TPS65217_DCDC_VOLT_SEL_1200MV;
usb_cur_lim = TPS65217_USB_INPUT_CUR_LIMIT_1300MA;
break;
case MPUPLL_M_600:
case MPUPLL_M_500:
case MPUPLL_M_300:
default:
mpu_vdd = TPS65217_DCDC_VOLT_SEL_1100MV;
usb_cur_lim = TPS65217_USB_INPUT_CUR_LIMIT_1300MA;
break;
}
if (tps65217_reg_write(TPS65217_PROT_LEVEL_NONE,
TPS65217_POWER_PATH,
usb_cur_lim,
TPS65217_USB_INPUT_CUR_LIMIT_MASK))
puts("tps65217_reg_write failure\n");
/* Set DCDC3 (CORE) voltage to 1.10V */
if (tps65217_voltage_update(TPS65217_DEFDCDC3,
TPS65217_DCDC_VOLT_SEL_1100MV)) {
puts("tps65217_voltage_update failure\n");
return;
}
/* Set DCDC2 (MPU) voltage */
if (tps65217_voltage_update(TPS65217_DEFDCDC2, mpu_vdd)) {
puts("tps65217_voltage_update failure\n");
return;
}
/*
* Set LDO3, LDO4 output voltage to 3.3V for Beaglebone.
* Set LDO3 to 1.8V and LDO4 to 3.3V for Beaglebone Black
* and PocketBeagle.
*/
if (board_is_bone() && !board_is_pb()) {
if (tps65217_reg_write(TPS65217_PROT_LEVEL_2,
TPS65217_DEFLS1,
TPS65217_LDO_VOLTAGE_OUT_3_3,
TPS65217_LDO_MASK))
puts("tps65217_reg_write failure\n");
} else {
if (tps65217_reg_write(TPS65217_PROT_LEVEL_2,
TPS65217_DEFLS1,
TPS65217_LDO_VOLTAGE_OUT_1_8,
TPS65217_LDO_MASK))
puts("tps65217_reg_write failure\n");
}
if (tps65217_reg_write(TPS65217_PROT_LEVEL_2,
TPS65217_DEFLS2,
TPS65217_LDO_VOLTAGE_OUT_3_3,
TPS65217_LDO_MASK))
puts("tps65217_reg_write failure\n");
}
void scale_vcores_generic(int freq)
{
int sil_rev, mpu_vdd;
/*
* The GP EVM, IDK and EVM SK use a TPS65910 PMIC. For all
* MPU frequencies we support we use a CORE voltage of
* 1.10V. For MPU voltage we need to switch based on
* the frequency we are running at.
*/
if (i2c_probe(TPS65910_CTRL_I2C_ADDR))
return;
/*
* Depending on MPU clock and PG we will need a different
* VDD to drive at that speed.
*/
sil_rev = readl(&cdev->deviceid) >> 28;
mpu_vdd = am335x_get_tps65910_mpu_vdd(sil_rev, freq);
/* Tell the TPS65910 to use i2c */
tps65910_set_i2c_control();
/* First update MPU voltage. */
if (tps65910_voltage_update(MPU, mpu_vdd))
return;
/* Second, update the CORE voltage. */
if (tps65910_voltage_update(CORE, TPS65910_OP_REG_SEL_1_1_0))
return;
}
void gpi2c_init(void)
{
/* When needed to be invoked prior to BSS initialization */
static bool first_time = true;
if (first_time) {
enable_i2c0_pin_mux();
i2c_init(CONFIG_SYS_OMAP24_I2C_SPEED,
CONFIG_SYS_OMAP24_I2C_SLAVE);
first_time = false;
}
}
void scale_vcores(void)
{
int freq;
gpi2c_init();
freq = am335x_get_efuse_mpu_max_freq(cdev);
if (board_is_beaglebonex())
scale_vcores_bone(freq);
else
scale_vcores_generic(freq);
}
void set_uart_mux_conf(void)
{
#if CONFIG_CONS_INDEX == 1
if (board_is_beaglelogic())
enable_uart4_pin_mux();
else
enable_uart0_pin_mux();
#elif CONFIG_CONS_INDEX == 2
enable_uart1_pin_mux();
#elif CONFIG_CONS_INDEX == 3
enable_uart2_pin_mux();
#elif CONFIG_CONS_INDEX == 4
enable_uart3_pin_mux();
#elif CONFIG_CONS_INDEX == 5
enable_uart4_pin_mux();
#elif CONFIG_CONS_INDEX == 6
enable_uart5_pin_mux();
#endif
}
void set_mux_conf_regs(void)
{
enable_board_pin_mux();
}
const struct ctrl_ioregs ioregs_evmsk = {
.cm0ioctl = MT41J128MJT125_IOCTRL_VALUE,
.cm1ioctl = MT41J128MJT125_IOCTRL_VALUE,
.cm2ioctl = MT41J128MJT125_IOCTRL_VALUE,
.dt0ioctl = MT41J128MJT125_IOCTRL_VALUE,
.dt1ioctl = MT41J128MJT125_IOCTRL_VALUE,
};
const struct ctrl_ioregs ioregs_bonelt = {
.cm0ioctl = MT41K256M16HA125E_IOCTRL_VALUE,
.cm1ioctl = MT41K256M16HA125E_IOCTRL_VALUE,
.cm2ioctl = MT41K256M16HA125E_IOCTRL_VALUE,
.dt0ioctl = MT41K256M16HA125E_IOCTRL_VALUE,
.dt1ioctl = MT41K256M16HA125E_IOCTRL_VALUE,
};
const struct ctrl_ioregs ioregs_evm15 = {
.cm0ioctl = MT41J512M8RH125_IOCTRL_VALUE,
.cm1ioctl = MT41J512M8RH125_IOCTRL_VALUE,
.cm2ioctl = MT41J512M8RH125_IOCTRL_VALUE,
.dt0ioctl = MT41J512M8RH125_IOCTRL_VALUE,
.dt1ioctl = MT41J512M8RH125_IOCTRL_VALUE,
};
const struct ctrl_ioregs ioregs = {
.cm0ioctl = MT47H128M16RT25E_IOCTRL_VALUE,
.cm1ioctl = MT47H128M16RT25E_IOCTRL_VALUE,
.cm2ioctl = MT47H128M16RT25E_IOCTRL_VALUE,
.dt0ioctl = MT47H128M16RT25E_IOCTRL_VALUE,
.dt1ioctl = MT47H128M16RT25E_IOCTRL_VALUE,
};
void sdram_init(void)
{
printf("SDRAM_INIT\n");
if (board_is_evm_sk()) {
/*
* EVM SK 1.2A and later use gpio0_7 to enable DDR3.
* This is safe enough to do on older revs.
*/
gpio_request(GPIO_DDR_VTT_EN, "ddr_vtt_en");
gpio_direction_output(GPIO_DDR_VTT_EN, 1);
}
if (board_is_icev2()) {
gpio_request(ICE_GPIO_DDR_VTT_EN, "ddr_vtt_en");
gpio_direction_output(ICE_GPIO_DDR_VTT_EN, 1);
}
if (board_is_evm_sk()) {
printf("EVM_SK\n");
config_ddr(303, &ioregs_evmsk, &ddr3_data,
&ddr3_cmd_ctrl_data, &ddr3_emif_reg_data, 0); }
else if (board_is_pb() || board_is_bone_lt() || board_is_beaglelogic()) {
printf("bone_lt\n");
config_ddr(400, &ioregs_bonelt,
&ddr3_beagleblack_data,
&ddr3_beagleblack_cmd_ctrl_data,
&ddr3_beagleblack_emif_reg_data, 0); }
else if (board_is_evm_15_or_later())
config_ddr(303, &ioregs_evm15, &ddr3_evm_data,
&ddr3_evm_cmd_ctrl_data, &ddr3_evm_emif_reg_data, 0);
else if (board_is_icev2())
config_ddr(400, &ioregs_evmsk, &ddr3_icev2_data,
&ddr3_icev2_cmd_ctrl_data, &ddr3_icev2_emif_reg_data,
0);
else if (board_is_gp_evm())
config_ddr(266, &ioregs, &ddr2_data,
&ddr2_cmd_ctrl_data, &ddr2_evm_emif_reg_data, 0);
else
config_ddr(266, &ioregs, &ddr2_data,
&ddr2_cmd_ctrl_data, &ddr2_emif_reg_data, 0);
}
#endif
#if !defined(CONFIG_SPL_BUILD) || \
(defined(CONFIG_SPL_ETH_SUPPORT) && defined(CONFIG_SPL_BUILD))
static void request_and_set_gpio(int gpio, char *name, int val)
{
int ret;
ret = gpio_request(gpio, name);
if (ret < 0) {
printf("%s: Unable to request %s\n", __func__, name);
return;
}
ret = gpio_direction_output(gpio, 0);
if (ret < 0) {
printf("%s: Unable to set %s as output\n", __func__, name);
goto err_free_gpio;
}
gpio_set_value(gpio, val);
return;
err_free_gpio:
gpio_free(gpio);
}
#define REQUEST_AND_SET_GPIO(N) request_and_set_gpio(N, #N, 1);
#define REQUEST_AND_CLR_GPIO(N) request_and_set_gpio(N, #N, 0);
/**
* RMII mode on ICEv2 board needs 50MHz clock. Given the clock
* synthesizer With a capacitor of 18pF, and 25MHz input clock cycle
* PLL1 gives an output of 100MHz. So, configuring the div2/3 as 2 to
* give 50MHz output for Eth0 and 1.
*/
static struct clk_synth cdce913_data = {
.id = 0x81,
.capacitor = 0x90,
.mux = 0x6d,
.pdiv2 = 0x2,
.pdiv3 = 0x2,
};
#endif
/*
* Basic board specific setup. Pinmux has been handled already.
*/
int board_init(void)
{
u32 sys_reboot;
sys_reboot = readl(PRM_RSTST);
if (sys_reboot & (1 << 9))
puts("Reset Source: IcePick reset has occurred.\n");
if (sys_reboot & (1 << 5))
puts("Reset Source: Global external warm reset has occurred.\n");
if (sys_reboot & (1 << 4))
puts("Reset Source: watchdog reset has occurred.\n");
if (sys_reboot & (1 << 1))
puts("Reset Source: Global warm SW reset has occurred.\n");
if (sys_reboot & (1 << 0))
puts("Reset Source: Power-on reset has occurred.\n");
#if defined(CONFIG_HW_WATCHDOG)
hw_watchdog_init();
#endif
gd->bd->bi_boot_params = CONFIG_SYS_SDRAM_BASE + 0x100;
#if defined(CONFIG_NOR) || defined(CONFIG_NAND)
gpmc_init();
#endif
#if !defined(CONFIG_SPL_BUILD) || \
(defined(CONFIG_SPL_ETH_SUPPORT) && defined(CONFIG_SPL_BUILD))
if (board_is_icev2()) {
int rv;
u32 reg;
REQUEST_AND_SET_GPIO(GPIO_PR1_MII_CTRL);
/* Make J19 status available on GPIO1_26 */
REQUEST_AND_CLR_GPIO(GPIO_MUX_MII_CTRL);
REQUEST_AND_SET_GPIO(GPIO_FET_SWITCH_CTRL);
/*
* Both ports can be set as RMII-CPSW or MII-PRU-ETH using
* jumpers near the port. Read the jumper value and set
* the pinmux, external mux and PHY clock accordingly.
* As jumper line is overridden by PHY RX_DV pin immediately
* after bootstrap (power-up/reset), we need to sample
* it during PHY reset using GPIO rising edge detection.
*/
REQUEST_AND_SET_GPIO(GPIO_PHY_RESET);
/* Enable rising edge IRQ on GPIO0_11 and GPIO 1_26 */
reg = readl(GPIO0_RISINGDETECT) | BIT(11);
writel(reg, GPIO0_RISINGDETECT);
reg = readl(GPIO1_RISINGDETECT) | BIT(26);
writel(reg, GPIO1_RISINGDETECT);
/* Reset PHYs to capture the Jumper setting */
gpio_set_value(GPIO_PHY_RESET, 0);
udelay(2); /* PHY datasheet states 1uS min. */
gpio_set_value(GPIO_PHY_RESET, 1);
reg = readl(GPIO0_IRQSTATUSRAW) & BIT(11);
if (reg) {
writel(reg, GPIO0_IRQSTATUS1); /* clear irq */
/* RMII mode */
printf("ETH0, CPSW\n");
} else {
/* MII mode */
printf("ETH0, PRU\n");
cdce913_data.pdiv3 = 4; /* 25MHz PHY clk */
}
reg = readl(GPIO1_IRQSTATUSRAW) & BIT(26);
if (reg) {
writel(reg, GPIO1_IRQSTATUS1); /* clear irq */
/* RMII mode */
printf("ETH1, CPSW\n");
gpio_set_value(GPIO_MUX_MII_CTRL, 1);
} else {
/* MII mode */
printf("ETH1, PRU\n");
cdce913_data.pdiv2 = 4; /* 25MHz PHY clk */
}
/* disable rising edge IRQs */
reg = readl(GPIO0_RISINGDETECT) & ~BIT(11);
writel(reg, GPIO0_RISINGDETECT);
reg = readl(GPIO1_RISINGDETECT) & ~BIT(26);
writel(reg, GPIO1_RISINGDETECT);
rv = setup_clock_synthesizer(&cdce913_data);
if (rv) {
printf("Clock synthesizer setup failed %d\n", rv);
return rv;
}
/* reset PHYs */
gpio_set_value(GPIO_PHY_RESET, 0);
udelay(2); /* PHY datasheet states 1uS min. */
gpio_set_value(GPIO_PHY_RESET, 1);
}
#endif
return 0;
}
#ifdef CONFIG_BOARD_LATE_INIT
int board_late_init(void)
{
#if !defined(CONFIG_SPL_BUILD)
uint8_t mac_addr[6];
uint32_t mac_hi, mac_lo;
#endif
#ifdef CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG
char *name = NULL;
if (board_is_bone_lt()) {
printf("BEAGLEBONEBLACK\n");
puts("Board: BeagleBone Black\n");
name = "A335BNLT";
/* BeagleBoard.org BeagleBone Black Wireless: */
if (!strncmp(board_ti_get_rev(), "BWA", 3)) {
name = "BBBW";
}
/* SeeedStudio BeagleBone Green Wireless */
if (!strncmp(board_ti_get_rev(), "GW1", 3)) {
name = "BBGW";
}
/* BeagleBoard.org BeagleBone Blue */
if (!strncmp(board_ti_get_rev(), "BLA", 3)) {
name = "BBBL";
}
/* SanCloud BeagleBone Enhanced */
if (!strncmp(board_ti_get_rev(), "SE", 2)) {
puts("Model: SanCloud BeagleBone Enhanced\n");
name = "SBBE";
}
/* Octavo Systems OSD3358-SM-RED */
if (!strncmp(board_ti_get_rev(), "OS00", 4)) {
puts("Model: Octavo Systems OSD3358-SM-RED\n");
name = "OS00";
}
}
if (board_is_bbg1())
name = "BBG1";
if (board_is_pb()) {
puts("Model: BeagleBoard.org PocketBeagle\n");
}
if (board_is_beaglelogic()) {
puts("Model: BeagleLogic\n");
}
set_board_info_env(name);
/*
* Default FIT boot on HS devices. Non FIT images are not allowed
* on HS devices.
*/
if (get_device_type() == HS_DEVICE)
env_set("boot_fit", "1");
#endif
#if !defined(CONFIG_SPL_BUILD)
/* try reading mac address from efuse */
mac_lo = readl(&cdev->macid0l);
mac_hi = readl(&cdev->macid0h);
mac_addr[0] = mac_hi & 0xFF;
mac_addr[1] = (mac_hi & 0xFF00) >> 8;
mac_addr[2] = (mac_hi & 0xFF0000) >> 16;
mac_addr[3] = (mac_hi & 0xFF000000) >> 24;
mac_addr[4] = mac_lo & 0xFF;
mac_addr[5] = (mac_lo & 0xFF00) >> 8;
if (!env_get("ethaddr")) {
printf("<ethaddr> not set. Validating first E-fuse MAC\n");
if (is_valid_ethaddr(mac_addr))
eth_env_set_enetaddr("ethaddr", mac_addr);
}
mac_lo = readl(&cdev->macid1l);
mac_hi = readl(&cdev->macid1h);
mac_addr[0] = mac_hi & 0xFF;
mac_addr[1] = (mac_hi & 0xFF00) >> 8;
mac_addr[2] = (mac_hi & 0xFF0000) >> 16;
mac_addr[3] = (mac_hi & 0xFF000000) >> 24;
mac_addr[4] = mac_lo & 0xFF;
mac_addr[5] = (mac_lo & 0xFF00) >> 8;
if (!env_get("eth1addr")) {
if (is_valid_ethaddr(mac_addr))
eth_env_set_enetaddr("eth1addr", mac_addr);
}
#endif
#ifdef CONFIG_ENV_VARS_UBOOT_RUNTIME_CONFIG
#ifdef CONFIG_TI_I2C_BOARD_DETECT
if (!board_is_pb() && !board_is_beaglelogic()) {
do_cape_detect();
}
#endif
#endif
return 0;
}
#endif
#ifndef CONFIG_DM_ETH
#if (defined(CONFIG_DRIVER_TI_CPSW) && !defined(CONFIG_SPL_BUILD)) || \
(defined(CONFIG_SPL_ETH_SUPPORT) && defined(CONFIG_SPL_BUILD))
static void cpsw_control(int enabled)
{
/* VTP can be added here */
return;
}
static struct cpsw_slave_data cpsw_slaves[] = {
{
.slave_reg_ofs = 0x208,
.sliver_reg_ofs = 0xd80,
.phy_addr = 0,
},
{
.slave_reg_ofs = 0x308,
.sliver_reg_ofs = 0xdc0,
.phy_addr = 1,
},
};
static struct cpsw_platform_data cpsw_data = {
.mdio_base = CPSW_MDIO_BASE,
.cpsw_base = CPSW_BASE,
.mdio_div = 0xff,
.channels = 8,
.cpdma_reg_ofs = 0x800,
.slaves = 1,
.slave_data = cpsw_slaves,
.ale_reg_ofs = 0xd00,
.ale_entries = 1024,
.host_port_reg_ofs = 0x108,
.hw_stats_reg_ofs = 0x900,
.bd_ram_ofs = 0x2000,
.mac_control = (1 << 5),
.control = cpsw_control,
.host_port_num = 0,
.version = CPSW_CTRL_VERSION_2,
};
#endif
#if ((defined(CONFIG_SPL_ETH_SUPPORT) || defined(CONFIG_SPL_USBETH_SUPPORT)) &&\
defined(CONFIG_SPL_BUILD)) || \
((defined(CONFIG_DRIVER_TI_CPSW) || \
defined(CONFIG_USB_ETHER) && defined(CONFIG_MUSB_GADGET)) && \
!defined(CONFIG_SPL_BUILD))
/*
* This function will:
* Read the eFuse for MAC addresses, and set ethaddr/eth1addr/usbnet_devaddr
* in the environment
* Perform fixups to the PHY present on certain boards. We only need this
* function in:
* - SPL with either CPSW or USB ethernet support
* - Full U-Boot, with either CPSW or USB ethernet
* Build in only these cases to avoid warnings about unused variables
* when we build an SPL that has neither option but full U-Boot will.
*/
int board_eth_init(bd_t *bis)
{
int rv, n = 0;
#if defined(CONFIG_USB_ETHER) && \
(!defined(CONFIG_SPL_BUILD) || defined(CONFIG_SPL_USBETH_SUPPORT))
uint8_t mac_addr[6];
uint32_t mac_hi, mac_lo;
/*
* use efuse mac address for USB ethernet as we know that
* both CPSW and USB ethernet will never be active at the same time
*/
mac_lo = readl(&cdev->macid0l);
mac_hi = readl(&cdev->macid0h);
mac_addr[0] = mac_hi & 0xFF;
mac_addr[1] = (mac_hi & 0xFF00) >> 8;
mac_addr[2] = (mac_hi & 0xFF0000) >> 16;
mac_addr[3] = (mac_hi & 0xFF000000) >> 24;
mac_addr[4] = mac_lo & 0xFF;
mac_addr[5] = (mac_lo & 0xFF00) >> 8;
#endif
#if (defined(CONFIG_DRIVER_TI_CPSW) && !defined(CONFIG_SPL_BUILD)) || \
(defined(CONFIG_SPL_ETH_SUPPORT) && defined(CONFIG_SPL_BUILD))
#ifdef CONFIG_DRIVER_TI_CPSW
if (!board_is_pb()) {
if (board_is_bone() || (board_is_bone_lt() && !board_is_bone_lt_enhanced() && !board_is_m10a()) ||
board_is_idk() || board_is_beaglelogic()) {
puts("eth0: MII MODE\n");
writel(MII_MODE_ENABLE, &cdev->miisel);
cpsw_slaves[0].phy_if = cpsw_slaves[1].phy_if =
PHY_INTERFACE_MODE_MII;
} else if (board_is_icev2()) {
puts("eth0: icev2: RGMII MODE\n");
writel(RMII_MODE_ENABLE | RMII_CHIPCKL_ENABLE, &cdev->miisel);
cpsw_slaves[0].phy_if = PHY_INTERFACE_MODE_RMII;
cpsw_slaves[1].phy_if = PHY_INTERFACE_MODE_RMII;
cpsw_slaves[0].phy_addr = 1;
cpsw_slaves[1].phy_addr = 3;
} else {
puts("eth0: RGMII MODE\n");
writel((RGMII_MODE_ENABLE | RGMII_INT_DELAY), &cdev->miisel);
cpsw_slaves[0].phy_if = cpsw_slaves[1].phy_if =
PHY_INTERFACE_MODE_RGMII;
}
rv = cpsw_register(&cpsw_data);
if (rv < 0)
printf("Error %d registering CPSW switch\n", rv);
else
n += rv;
}
#endif
/*
*
* CPSW RGMII Internal Delay Mode is not supported in all PVT
* operating points. So we must set the TX clock delay feature
* in the AR8051 PHY. Since we only support a single ethernet
* device in U-Boot, we only do this for the first instance.
*/
#define AR8051_PHY_DEBUG_ADDR_REG 0x1d
#define AR8051_PHY_DEBUG_DATA_REG 0x1e
#define AR8051_DEBUG_RGMII_CLK_DLY_REG 0x5
#define AR8051_RGMII_TX_CLK_DLY 0x100
if (board_is_evm_sk() || board_is_gp_evm() || board_is_bone_lt_enhanced() || board_is_m10a()) {
const char *devname;
devname = miiphy_get_current_dev();
miiphy_write(devname, 0x0, AR8051_PHY_DEBUG_ADDR_REG,
AR8051_DEBUG_RGMII_CLK_DLY_REG);
miiphy_write(devname, 0x0, AR8051_PHY_DEBUG_DATA_REG,
AR8051_RGMII_TX_CLK_DLY);
}
#endif
#if defined(CONFIG_USB_ETHER) && \
(!defined(CONFIG_SPL_BUILD) || defined(CONFIG_SPL_USBETH_SUPPORT))
if (is_valid_ethaddr(mac_addr))
eth_env_set_enetaddr("usbnet_devaddr", mac_addr);
rv = usb_eth_initialize(bis);
if (rv < 0)
printf("Error %d registering USB_ETHER\n", rv);
else
n += rv;
#endif
return n;
}
#endif
#endif /* CONFIG_DM_ETH */
#ifdef CONFIG_SPL_LOAD_FIT
int board_fit_config_name_match(const char *name)
{
//FIME: we currently dont use this, yet...
if (board_is_gp_evm() && !strcmp(name, "am335x-evm"))
return 0;
else if (board_is_pb() && !strcmp(name, "am335x-pocketbeagle"))
return 0;
else if (board_is_beaglelogic() && !strcmp(name, "am335x-beaglelogic"))
return 0;
else if (board_is_os00() && !strcmp(name, "am335x-boneblack"))
return 0;
else if (board_is_bone() && !strcmp(name, "am335x-bone"))
return 0;
else if (board_is_bone_lt() && !strcmp(name, "am335x-boneblack"))
return 0;
else if (board_is_evm_sk() && !strcmp(name, "am335x-evmsk"))
return 0;
else if (board_is_bbg1() && !strcmp(name, "am335x-bonegreen"))
return 0;
else if (board_is_icev2() && !strcmp(name, "am335x-icev2"))
return 0;
else
return -1;
}
#endif
#ifdef CONFIG_TI_SECURE_DEVICE
void board_fit_image_post_process(void **p_image, size_t *p_size)
{
secure_boot_verify_image(p_image, p_size);
}
#endif
#if !CONFIG_IS_ENABLED(OF_CONTROL)
static const struct omap_hsmmc_plat am335x_mmc0_platdata = {
.base_addr = (struct hsmmc *)OMAP_HSMMC1_BASE,
.cfg.host_caps = MMC_MODE_HS_52MHz | MMC_MODE_HS | MMC_MODE_4BIT,
.cfg.f_min = 400000,
.cfg.f_max = 52000000,
.cfg.voltages = MMC_VDD_32_33 | MMC_VDD_33_34 | MMC_VDD_165_195,
.cfg.b_max = CONFIG_SYS_MMC_MAX_BLK_COUNT,
};
U_BOOT_DEVICE(am335x_mmc0) = {
.name = "omap_hsmmc",
.platdata = &am335x_mmc0_platdata,
};
static const struct omap_hsmmc_plat am335x_mmc1_platdata = {
.base_addr = (struct hsmmc *)OMAP_HSMMC2_BASE,
.cfg.host_caps = MMC_MODE_HS_52MHz | MMC_MODE_HS | MMC_MODE_8BIT,
.cfg.f_min = 400000,
.cfg.f_max = 52000000,
.cfg.voltages = MMC_VDD_32_33 | MMC_VDD_33_34 | MMC_VDD_165_195,
.cfg.b_max = CONFIG_SYS_MMC_MAX_BLK_COUNT,
};
U_BOOT_DEVICE(am335x_mmc1) = {
.name = "omap_hsmmc",
.platdata = &am335x_mmc1_platdata,
};
#endif