Part Number: AM3354
Other Parts Discussed in Thread: AM3354
Hi ,
SDK: ti-processor-sdk-linux-rt-am335x-evm-03.03.00.04-Linux-x86-Install.bin
Main chip : am3354
Device tree : am335x-boneblack.dtb
Board is customized by our company.
Use the USB virtual serial port function to load the drive sequence:
modprobe g_ether
modprobe g_serial
When I open the serial debugging assistant, it will receive debug (UART0) port information. As shown below:
Why is there a debug (UART0) port message when using the g_serial driver ?
How can I not receive the debug (UART0) port message when using the g_serial driver?