Part Number: AMIC110
Tool/software: TI-RTOS
There was a post from 2016 (e2e.ti.com/.../514649)which was never solved.
Because I had the same problem, I will tell how to solve ;)
The solution is, don't put this code to "AddWebFiles()". Better is to span a new task, let it wait until everyhting is initialized. Than add the Username and Password to the configuration.
So here is my code:
void meinTest(void) {
volatile Handle hCfg;
volatile int valid;
CI_ACCT CA
hCfg = CfgGetDefault();
// Creates the Authorization Realm 1
//valid = CfgAddEntry(hCfg, CFGTAG_SYSINFO, CFGITEM_SYSINFO_REALM1, 0, 7, (UINT8 *)"REALM1", 0);
strcpy(CA.Username, "Stefan");
strcpy(CA.Password, "geheim");
CA.Flags = CFG_ACCTFLG_CH1; // Adds the user the the Realm 1
valid = CfgAddEntry(hCfg, CFGTAG_ACCT, CFGITEM_ACCT_REALM, 0, sizeof(CI_ACCT), (UINT8 *)&CA, 0);
}